This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pull-up resistor on Memory TQ pin.



Why Mistral EVM use Pull-up resistor (R57, 10K to VIO) on OMAP AH11 ball (feed-thru to AC9 top ball). Micron POP memory (MT29C4G48MAZAPAKQ-5 IT) AC9 ball is named TQ pin. TQ is HIGH when LPDDR TJ exceeds 85C. (TQ is Temperature Sensor Output pin).

  • Which version of the schematics for the processor module are you referencing?

    Looking at the latest schematics from Mistral's website for the processor module (0.4mm with POP), AH11 goes into a 0 ohm resistor that is designated as "DNI" or Do Not Install.  Secondly, the other end of that resistor is floating.