Other Parts Discussed in Thread: OMAP3530, TPS65950
What is the functionality of SYS_DRM_MSECURE input pin in OMAP3530?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Meir:
Please refer to the following post which addresses the same question:
http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/p/71883/261019.aspx#261019
Best Regards,
Michael T
PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question. Thanks!
Hi Michael,
According to OMAP3530/25 Application Processor, SPRS507F–FEBRUARY 2008–REVISED OCTOBER 2009, Page 44, (CBB pacage), SYS_DRM_MSECURE, AF9 ball is input to OMAP.
According to your answer it is OUTPUT from OMAP.
Regards,
Meir
Meir:
That is an error in the data manual. SYS_DRM_MSECURE is an output. Below is the complete list of corrections that will be made to
the data manual Ball Characteristics tables when the data manual is updated.
CBB Ball Table
I/O Type Corrections:
sys_drm_secure I => O
mcbsp3_dr O => I
husb3_tll_stp IO => I
husb3_tll_dir IO => O
husb3_tll_nxt IO => O
tv_out1 O => AO
tv_out2 O => AO
CBC Ball Table
Ball ID Corrections:
Bottom: AD7 Top: AA5 sys_nreswarm, gpio_30, safe_mode => Change top ball ID from AA5 to NA.
I/O Type Corrections:
husb3_tll_nxt IO => O
tv_vfb1 O => AO
tv_vfb2 O => AO
tv_vref I => AO
CUS Ball Table
I/O Type Corrections:
mcbsp3_dr O => I
Regards,
Michael T
Hi,
Can you please say why on Mistral EVM board the TPS65950 MSECURE H8 ball is connected to OMAP3530DCBBA K8 ball (GPIO_64).
It is also connected to OMAP3530 AF9 ball (SYS_DRM_MSECURE, GPIO_22) thru not-placed serial resistor.
Why do Mistral prefer to use GPIO_64 instead of GPIO_22?
Thanks,
Meir
Meir:
Normally GPIO64 is used to read the state of SYS_DRM_SECURE. If the design is not using the SYS_DRM_SECURE signal, H8 can be used as a general-purpose I/O pin (GPIO22) by changing the pin mux setting.
regards,
Michael T
PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question. Thanks!
Meir:
On our OMAP3530 processor module (Rev C) AF9 goes to a zero-ohm not-installed resistor. If that resistor is installed it goes to GPIO_64 (K8).
Instead AF9 connects thru a zero-ohm resistor to ETK_D8. The pin mux for AF9 by normally outputs the ETK_D8 signal. AF9 can also be pin muxed
to be GPIO_22, but I don't see GPIO_22 used in our schematic.
Regards,
Michael T
PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question. Thanks!