Team, can you please point me to the pre-loaded example that comes with the ICE EVM. As mentioned in section 8.1 of the EVM guide, there is a default image. Is the source project in the SDK and if so which (Linux, RT Linux, or RTOS)? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team, can you please point me to the pre-loaded example that comes with the ICE EVM. As mentioned in section 8.1 of the EVM guide, there is a default image. Is the source project in the SDK and if so which (Linux, RT Linux, or RTOS)? Thanks.
Hi Deep,
The AM3359 ICE development board comes pre-loaded with a default application in the on-board SPI flash device. This application is most probably based on RTOS package, but you can check that through examine the boot messages you have. That might be EtherCAT industrial application, but if you can provide the console output you have, we can be more specific.
Check also below e2e thread:
Regards,
Pavel