This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Windows development for C6A816x

In the release notes, it states "this release only supports Ubuntu 10.04 LTS 32-bit as your development host."  Are there plans to implement a development platform under Windows?

  • Alex Barry said:
    In the release notes, it states "this release only supports Ubuntu 10.04 LTS 32-bit as your development host."  Are there plans to implement a development platform under Windows?

    Currently the only supported target OS for the C6A816x is Linux, and there are no plans I am aware of to support development for a Linux target on a Windows PC host directly (in general it is impractical to develop for Linux on Windows). Though I am not sure of the schedule off hand, I suspect there will be alternative OSes available in the future (such as Windows CE in particular) that may be more practical for Windows PC host development.

    If you require a Windows host for development, you can use a virtual Linux machine (i.e. VMWare, Virtualbox, etc.) for development. Using a virtual machine is a common practice, since it lets you have practically two machines in one, however in general for long term development I personally prefer having a dedicated Linux machine (due to speed, persistence, reliability, etc).

  • Yes, the current projection is that WinCE support will become available in 2Q 2011.

    Regards,
    Marc