Part Number: AM4372
Other Parts Discussed in Thread: AM4376
Sitara support team,
I would like to make sure that the following NOR Flash Memory can use a qspi boot for AM4376.
MICRON: MT25QL512ABB1EW9-0SIT
I have checked Section 5.2.6.7.1.in AM437x TRM and there is described...
-The boot device must default to quad mode, if quad-read support is desired
However MT25QL512ABB1EW9-0SIT is set "Quad I/O protocol" bit in Nonvolatile Configuration Register is "1 = Disabled (Default)".
Is this problem for using the NOR Flash Memory? Or is it not problem to use if "Quad I/O protocol" bit is set "0 = enabled"?
If there are any other limitations to use the NOR Flash Memory, please let me know.
Best regards,
Kanae