Part Number: AM4376
Other Parts Discussed in Thread: AM4372
Hi,
I browsed forum but cannot find exact response to my issues. IIRC L3 interconnect is not available so cannot really understand what is going on.
I have this in my bootlog:
NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations cpuidle: using governor ladder cpuidle: using governor menu ------------[ cut here ]------------ WARNING: CPU: 0 PID: 1 at /kernel-source//drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x2e0/0x344 44000000.ocp:L3 Custom Error: MASTER M2 (64-bit) TARGET GPMC (Read): Data Access in User mode during Debug access Modules linked in: CPU: 0 PID: 1 Comm: swapper Not tainted 4.12.28-wifi-emc-dut #6 Hardware name: Generic AM43 (Flattened Device Tree) [<c010fa08>] (unwind_backtrace) from [<c010c45c>] (show_stack+0x20/0x24) [<c010c45c>] (show_stack) from [<c04cc0d4>] (dump_stack+0x20/0x28) [<c04cc0d4>] (dump_stack) from [<c01324ac>] (__warn+0xec/0x108) [<c01324ac>] (__warn) from [<c0132510>] (warn_slowpath_fmt+0x48/0x50) [<c0132510>] (warn_slowpath_fmt) from [<c04fe370>] (l3_interrupt_handler+0x2e0/0x344) [<c04fe370>] (l3_interrupt_handler) from [<c0170fac>] (__handle_irq_event_percpu+0xd4/0x238) [<c0170fac>] (__handle_irq_event_percpu) from [<c017113c>] (handle_irq_event_percpu+0x2c/0x68) [<c017113c>] (handle_irq_event_percpu) from [<c01711e4>] (handle_irq_event+0x6c/0x90) [<c01711e4>] (handle_irq_event) from [<c0174a9c>] (handle_fasteoi_irq+0xc4/0x164) [<c0174a9c>] (handle_fasteoi_irq) from [<c01701d0>] (generic_handle_irq+0x28/0x38) [<c01701d0>] (generic_handle_irq) from [<c0170838>] (__handle_domain_irq+0xc0/0xdc) [<c0170838>] (__handle_domain_irq) from [<c0101544>] (gic_handle_irq+0x60/0x8c) [<c0101544>] (gic_handle_irq) from [<c093108c>] (__irq_svc+0x6c/0xa8) Exception stack(0xef11db58 to 0xef11dba0) db40: ef1c3300 ef1f4b80 db60: 00000000 00000000 ef1f4b80 ef1c3300 00000000 00000000 00000015 ef1c3338 db80: 60000013 ef11dbdc ef11dba8 ef11dba8 c0172ddc c0172d18 60000013 ffffffff [<c093108c>] (__irq_svc) from [<c0172d18>] (__setup_irq+0x548/0x66c) [<c0172d18>] (__setup_irq) from [<c0172fbc>] (request_threaded_irq+0xc4/0x17c) [<c0172fbc>] (request_threaded_irq) from [<c0175730>] (devm_request_threaded_irq+0x7c/0xb8) [<c0175730>] (devm_request_threaded_irq) from [<c04fe508>] (omap_l3_probe+0x134/0x214) [<c04fe508>] (omap_l3_probe) from [<c05d81fc>] (platform_drv_probe+0x60/0xac) [<c05d81fc>] (platform_drv_probe) from [<c05d63d4>] (driver_probe_device+0x214/0x2dc) [<c05d63d4>] (driver_probe_device) from [<c05d6644>] (__device_attach_driver+0xa4/0xbc) [<c05d6644>] (__device_attach_driver) from [<c05d4700>] (bus_for_each_drv+0x98/0xa0) [<c05d4700>] (bus_for_each_drv) from [<c05d6108>] (__device_attach+0xac/0x114) [<c05d6108>] (__device_attach) from [<c05d6678>] (device_initial_probe+0x1c/0x20) [<c05d6678>] (device_initial_probe) from [<c05d56a0>] (bus_probe_device+0x38/0x90) [<c05d56a0>] (bus_probe_device) from [<c05d3880>] (device_add+0x414/0x514) [<c05d3880>] (device_add) from [<c0729050>] (of_device_add+0x44/0x48) [<c0729050>] (of_device_add) from [<c07295a8>] (of_platform_device_create_pdata+0x94/0xc4) [<c07295a8>] (of_platform_device_create_pdata) from [<c0729680>] (of_platform_bus_create+0x84/0x1f8) [<c0729680>] (of_platform_bus_create) from [<c072996c>] (of_platform_populate+0x84/0xd8) [<c072996c>] (of_platform_populate) from [<c0e0fc24>] (pdata_quirks_init+0x68/0xa0) [<c0e0fc24>] (pdata_quirks_init) from [<c0e0f70c>] (omap_generic_init+0x1c/0x28) [<c0e0f70c>] (omap_generic_init) from [<c0e03ac4>] (customize_machine+0x2c/0x38) [<c0e03ac4>] (customize_machine) from [<c0101bf0>] (do_one_initcall+0x134/0x15c) [<c0101bf0>] (do_one_initcall) from [<c0e00f88>] (kernel_init_freeable+0x1d4/0x290) [<c0e00f88>] (kernel_init_freeable) from [<c092b5e8>] (kernel_init+0x18/0x11c) [<c092b5e8>] (kernel_init) from [<c0107b08>] (ret_from_fork+0x14/0x2c) ---[ end trace ca236957eef2cfb1 ]--- OMAP GPIO hardware version 0.1
So from above error message it seems that GPMC is trying to read something but in dts we have gpmc disabled (we don't use it we use eMMC and sdio). Is there any chance to get more insight what does this warning means (board normally boots and works just having warning in bootlog is not nice ;)).
Thanks,
marek