Part Number: PROCESSOR-SDK-OMAPL138
Hi,
Some novice questions.
We're upgrading from mcsdk_1_01_00_02 to ti-processor-sdk-linux-omapl138-lcdk-06.00.00.07. and have been studying docs/06_00_00_07/linux/Overview.html and related. We've downloaded and installed ...install.bin for RTOS and Linux. We've successfully built Linux and uBoot for LCDK with defaults - OK. I would like to ask few basic questions to verify if we're on right path, HW is custom and has major differences to LCDK:
- top level Makefile makes with 'tisdk_omapl138-lcdk_defconfig' and skips .config which we' ve just reconfigured - which is the right way to customize configuration
- Which is recommended RFS, 'arago-base-tisdk-image-omapl138-lcdk' or??
- How can we forward 'install' there?
- We need wpa_supplicant and gstreamer with related drivers, are they included in some of those filesystems or should we build and install them 'manually'?
We would like to minimize our effort to this upgrade as our resources are involved in application. Are there parties which could do this configuration with USD?
Best regards,
ristoH