Part Number: AM5749
I have tested the the SSD example in AM5749 and the speed is 150ms. But when I migrant the model from 728*360 to 256*256, the speed is 1700ms. Is there some rules for model size?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5749
I have tested the the SSD example in AM5749 and the speed is 150ms. But when I migrant the model from 728*360 to 256*256, the speed is 1700ms. Is there some rules for model size?
Hi,
When the feature map size is smaller than 64x64, you need to set the configuration for conv2dkernelype parameter as dense (1) during the import process. This parameter is applicable on per layer basis (multiple values are expected - as many as there are layers).
This configuration will be automated during import process in Processor SDK 6.1 release expected to happen Oct end, 2019.
Regards,
Manisha