This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Have anyone used DM6446 SPI two CS signals (EN0 and EN1)?



Hi,

Have anyone used DM6446 SPI two CS signals? 

According to DM644x SPI U/G (SPRUE32A), DM6446 SPI has the ability to control two slave devices using the signals (SPI_EN0 and SPI_EN1).
I'm planning to use the ability now.

I'd like to get the information about someone using it successfully.  

Thanks in advance for your information.

Best regards,
j-breeze