Part Number: AM4379
Other Parts Discussed in Thread: SYSBIOS, AMIC110,
Hi,
We are working on AM437x-IDK (SD Card boot).
We don't use QSPI Flash because our custom board is designed without QSPI Flash.
PDK Version : pdk_am437x_1_0_15
Sysbios Version : bios_6_75_02_00
We build the Eathercat application from PRU-ICSS-EtherCAT_Slave_01.00.07.02 SDK. I successfully compiled and run the application in AM437x-IDK on DDR.
But our end application is board should work in on-chip RAM, so we followed this document SPRAC45A and build application for on-chip RAM(L3 Build).
But the application is not running on board we made the following changes for memory segments.
For testing, we changed the memory segment like below and the application is booting fine.
Since we need OCMCRAM because our application size gets increases after integrating all features.
Kindly help us to resolve this issue.
Regards,
Ravi