dear all
Linux Kernel v2.6.10_mvl401 Configuration have
[ ] Disable I-Cache [ ] Disable D-Cache however Linux Kernel v2.6.14_mvl401-davinci_evm Configuration do not have
[ ] Disable I-Cache [ ] Disable D-Cache
question:how to join file to make
Linux Kernel v2.6.14_mvl401-davinci_evm Configuration have
Tel:021-64320376
laibaotang
as follows:
Linux Kernel v2.6.14_mvl401-davinci_evm Configuration
──────────────────────────────────────────────────────────────────────────────
┌─────────────────────── System type and features ────────────────────────┐
│ Arrow keys navigate the menu. <Enter> selects submenus --->. │
│ Highlighted letters are hotkeys. Pressing <Y> includes, <N> excludes, │
│ <M> modularizes features. Press <Esc><Esc> to exit, <?> for Help, </> │
│ for Search. Legend: [*] built-in [ ] excluded <M> module < > │
│ ┌─────────────────────────────────────────────────────────────────────┐ │
│ │ ARM system type (RiscPC) ---> │ │
│ │--- Processor Type │ │
│ │[ ] Support ARM610 processor (NEW) │ │
│ │[ ] Support ARM710 processor (NEW) │ │
│ │[ ] Support StrongARM(R) SA-110 processor (NEW) │ │
│ │--- Processor Features │ │
│ │[*] Use the ARM EABI to compile the kernel (NEW) │ │
│ │[*] Allow old ABI binaries to run with this kernel (EXPERIMENTAL) (│ │
│ │(0) Compressed ROM boot loader base address (NEW) │ │
│ │(0) Compressed ROM boot loader BSS address (NEW) │ │
│ └┴(+)─────────────────────────────────────────────────────────────────┘ │
├─────────────────────────────────────────────────────────────────────────┤
│ <Select> < Exit > < Help >
Linux Kernel v2.6.10_mvl401 Configuration
──────────────────────────────────────────────────────────────────────────────
┌─────────────────────── System type and features ────────────────────────┐
│ Arrow keys navigate the menu. <Enter> selects submenus --->. │
│ Highlighted letters are hotkeys. Pressing <Y> includes, <N> excludes, │
│ <M> modularizes features. Press <Esc><Esc> to exit, <?> for Help, </> │
│ for Search. Legend: [*] built-in [ ] excluded <M> module < > │
│ ┌─────────────────────────────────────────────────────────────────────┐ │
│ │ ARM system type (TI DaVinci) ---> │ │
│ │ TI DaVinci Implementations ---> │ │
│ │--- Processor Type │ │
│ │--- Processor Features │ │
│ │--- Support Thumb user binaries │ │
│ │[ ] Disable I-Cache │ │
│ │[ ] Disable D-Cache │ │
│ │[ ] Force write through D-cache │ │
│ │[ ] Round robin I and D cache replacement algorithm │ │
│ │[*] Use the ARM EABI to compile the kernel │ │
│ └┴(+)─────────────────────────────────────────────────────────────────┘ │
├─────────────────────────────────────────────────────────────────────────┤
│ <Select> < Exit > < Help >