After following the out of box start up guide for this product and not having any luck (it would say boot complete and give the correct BMC version, but for my IP address it just said "emon") I contacted TI support and left a ticket. They instructed me to follow those steps only after connecting to the serial UART and running the command 'minicom -D /dev/ttyUSB1'. This is where I am getting stuck and need help. The PC that I am connecting the board to is a windows 10 device, so I can't run that Linux command, when I log into the board on my PuTTy terminal and try to run the command, it does not recognize 'minicom'... So I am assuming it is a package I would have to download and maybe TFTP over to the board. If one of the SME's on this board could give me some insight on how to get the IP address to display so I can put it into a web browser that would be great.