This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5158 and DM365, lack of Cr component

Other Parts Discussed in Thread: TVP5158

Hi,

I developed a proprietary board based upon DM365 UdWorks RDK. Video front end consists of a DM365 coupled with a single TVP5158 video decoder connected as in UdWork schematic except of slave video decoder.

I used mcvip_test.out application to display the captured video using option 5 (4 channel in CIF format) but the image lacked of red components, so I forced "blue" screen output from TVP5158 setting registers as follows:
reg 0xA9 = 0x08
reg 0x90 = 0x80 (Y component)
reg 0x91 = 0x40 (Cb component)
reg 0x92 = 0x20 (Cr component)

Checking TVP5158 output with oscilloscope I don't see any output of  Cr component and also, saving frames on file there's no Cr component.

This is YUVIN_0000_384x288.BIN first line: 40 80 40 80 40 80 40 80 40 80 40 80 40 80 40 80 ...

Any suggestions?

Thanks in advance.

Stefano