Hi there,
on the eval board (TMDXICE110-BTA) is the power for VDDS derived from da dedicated LDO (1V8_2). According to the datasheet (SPRS971C chapter 6) it is also possible using just one 1V8 for powering all 1.8V AMIC110 supplies - am I correct?
from the datasheet:
B. When using the ZCZ package option, VDD_MPU and VDD_CORE power inputs may be powered from the same
source if the application only uses operating performance points (OPPs) that define a common power supply voltage
for VDD_MPU and VDD_CORE. The ZCE package option has the VDD_MPU domain merged with the VDD_CORE
domain.
the AMIC110 comes only in the ZCZ package option and the ZCE package option is not avilable - isn't it so?
if the application only uses operating performance points (OPPs) that define a common power supply voltage
for VDD_MPU and VDD_CORE
where do I find this information on which OPPs the AMIC is configured?
or where/how can I set this OPP mode?