This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiling GLCD driver for OMAPL138

Other Parts Discussed in Thread: OMAPL138

hi..

Im getting the following errors, when i'm compiling the GLCD drivers for OMAPL138

root@vijay-Z460:/home/vijay/Desktop/test# make

make -C /lib/modules/2.6.32-26-generic/build M=/home/vijay/Desktop/test modules

make[1]: Entering directory `/usr/src/linux-headers-2.6.32-26-generic'

  CC [M]  /home/vijay/Desktop/test/fbuffL138.o

/home/vijay/Desktop/test/fbuffL138.c:101:31: error: asm/mach/cputype.h: No such file or directory

/home/vijay/Desktop/test/fbuffL138.c:102:26: error: asm/mach/io.h: No such file or directory

/home/vijay/Desktop/test/fbuffL138.c:103:32: error: asm/mach/hardware.h: No such file or directory

/home/vijay/Desktop/test/fbuffL138.c: In function ‘lcdc_read’:

/home/vijay/Desktop/test/fbuffL138.c:176: warning: passing argument 1 of ‘__readl’ makes pointer from integer without a cast

/usr/src/linux-headers-2.6.32-26-generic/arch/x86/include/asm/io.h:26: note: expected ‘const volatile void *’ but argument is of type ‘resource_size_t’

/home/vijay/Desktop/test/fbuffL138.c: In function ‘lcdc_write’:

/home/vijay/Desktop/test/fbuffL138.c:181: warning: passing argument 2 of ‘__writel’ makes pointer from integer without a cast

/usr/src/linux-headers-2.6.32-26-generic/arch/x86/include/asm/io.h:34: note: expected ‘volatile void *’ but argument is of type ‘resource_size_t’

/home/vijay/Desktop/test/fbuffL138.c: In function ‘lcd_disable_raster’:

/home/vijay/Desktop/test/fbuffL138.c:276: warning: suggest parentheses around operand of ‘!’ or change ‘&’ to ‘&&’ or ‘!’ to ‘~’

/home/vijay/Desktop/test/fbuffL138.c:276: warning: suggest parentheses around operand of ‘!’ or change ‘&’ to ‘&&’ or ‘!’ to ‘~’

make[2]: *** [/home/vijay/Desktop/test/fbuffL138.o] Error 1

make[1]: *** [_module_/home/vijay/Desktop/test] Error 2

make[1]: Leaving directory `/usr/src/linux-headers-2.6.32-26-generic'

make: *** [default] Error 2