Other Parts Discussed in Thread: UNIFLASH
Hi
I have questions which relates with following E2E thread
Q1: When I tried to program FlashWriter on Target by using latest Uniflash v5.1.0, the character "C" was not printed on COM port.
If I switched the version of Uniflash (e.g. 4.6.0 or 5.0.0) then the character "C" was printed on COM port.
Please check and modify the latest tool if it 's not correct one.
Q2: After programming FlashWrite on Target by using Uniflash (v4.6.0 or 5.0.0), I tried to flash the program on OSPI with the following steps:
dslite.bat --mode processors -c COM15 -e 10000 -d 3 -o 0
dslite.bat --mode processors -c COM15 -f c:\ti\pdk_am65xx_1_0_5\packages\ti\boot\sbl\binary\am65xx_evm\ospi\bin\sbl_ospi_img_mcu1_0_release.tiimage -d 3 -o 0
dslite.bat --mode processors -c COM15 -f c:\ti\pdk_am65xx_1_0_5\packages\ti\drv\sciclient\soc\V0\sysfw.bin -d 3 -o 40000
......
Erase was completed correctly.
However, flashing was failed.
Error message is:
=========================================-
C:\ti\uniflash_4.6.0>dslite.bat --mode processors -c COM15 -f c:\ti\pdk_am65xx_1_0_5\packages\ti\boot\sbl\binary\am65xx_evm\ospi\bin\sbl_ospi_img_mcu1_0_release.tiimage -d 3 -o 0
Executing the following command:
> C:\ti\uniflash_4.6.0\processors\ProcessorSDKSerialFlash.exe -c COM15 -f c:\ti\pdk_am65xx_1_0_5\packages\ti\boot\sbl\binary\am65xx_evm\ospi\bin\sbl_ospi_img_mcu1_0_release.tiimage -d 3 -o 0
For more details and examples, please visit processors.wiki.ti.com/.../UniFlash_v4_Quick_Guide
----------------------------------------------------------------------------
ProcessorSDKSerialFlash CLI Tool
Copyright (C) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/
Version 1.0.0.5
----------------------------------------------------------------------------
Flashing Image to Flash Writer..
Transferring Header information..
Header Transfer complete!
Transferring File of size 150990 bytes
File Transfer complete!
Programming Flash Device..
Flash Programming Failed!!
=========================================-
Are you able to flash the image on OSPI?
Which version of tools (CCS, PDK, Uniflash e.t.c.) are you using?
Thanks and Best regards,
HaTa.