Part Number: AM5726
Other Parts Discussed in Thread: AM5728, , BEAGLEBOARD-X15, DRA752
Hello
I have a custom board based on beagle-x15/ti-evm.
I have make some modifications on U-boot, for example my custom board dont have an EEPROM to detect the board.
If I start the board I get some u-boot messages and it seems look it want to start the kernel but it stuck.
U-Boot SPL 2019.01 (Oct 16 2019 - 17:50:53 +0200) DRA752-GP ES2.0 Trying to boot from MMC1 no pinctrl state for default mode no pinctrl state for default mode Loading Environment from FAT... *** Warning - bad CRC, using default environment Loading Environment from MMC... Card did not respond to voltage select! *** Warning - No block device, using default environment U-Boot 2019.01 (Oct 16 2019 - 17:50:53 +0200) CPU : DRA752-GP ES2.0 Model: TI AM5728 BeagleBoard-X15 Board: SEC4 DRAM: 1 GiB Size of DRAM is 1024 MB beagle_x MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Loading Environment from FAT... *** Warning - bad CRC, using default environment Loading Environment from MMC... Card did not respond to voltage select! *** Warning - No block device, using default environment *** -> This Board is unknown late init late init 2a Card did not respond to voltage select! invalid mmc device late init 2b end of late init Net: Could not get PHY for ethernet@48484000: addr 1 Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Unable to read file boot.scr ** 1490 bytes read in 2 ms (727.5 KiB/s) Loaded env from uEnv.txt Importing environment from mmc0 ... Running uenvcmd ... 1 bytes read in 1 ms (1000 Bytes/s) Already setup. switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 4211200 bytes read in 190 ms (21.1 MiB/s) 133193 bytes read in 8 ms (15.9 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffdc000, end 8ffff848 ... OK Starting kernel ...
The printenv:
=> printenv
arch=arm
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
baudrate=115200
board=am57xx
board_name=beagle_x15
board_rev=0.0
board_serial=0000
boot_fdt=try
boot_fit=0
bootargs=androidboot.serialno=${serial#} console=ttyS2,115200 androidboot.console=ttyS2 androidboot.hardware=beagle_x15board
bootcmd=if test ${dofastboot} -eq 1; then echo Boot fastboot requested, resetting dofastboot ...;setenv dofastboot 0; saveenv;echo Booting
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootfile=zImage
bootm_size=0x10000000
bootpart=0:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyO2,115200n8
cpu=armv7
dfu_alt_info_emmc=rawemmc raw 0 3751936;boot part 1 1;rootfs part 1 2;MLO fat 1 1;MLO.raw raw 0x100 0x200;u-boot.img.raw raw 0x300 0x1000;1
dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x200;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x1
dfu_alt_info_qspi=MLO raw 0x0 0x040000;u-boot.img raw 0x040000 0x0100000;u-boot-spl-os raw 0x140000 0x080000;u-boot-env raw 0x1C0000 0x0100
dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x4000000
dfu_bufsiz=0x10000
dofastboot=0
emmc_android_boot=echo Trying to boot Android from eMMC ...; run update_to_fit; setenv eval_bootargs setenv bootargs $bootargs; run eval_b;
emmc_linux_boot=echo Trying to boot Linux from eMMC ...; setenv mmcdev 1; setenv bootpart 1:2; setenv mmcroot /dev/mmcblk0p2 rw; run mmcbo;
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if ru;
ethaddr=18:62:e4:6f:58:2c
fastboot.board_rev=0.0
fastboot.cpu=DRA752
fastboot.secure=GP
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtcontroladdr=bdf25650
fdtfile=undefined
findfdt=if test $board_name = omap5_uevm; then setenv fdtfile omap5-uevm.dtb; fi; if test $board_name = dra7xx; then setenv fdtfile dra7-e
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage
fit_loadaddr=0x90000000
get_overlaystring=for overlay in $overlay_files;do;setenv overlaystring ${overlaystring}'#'${overlay};done;
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
kernel_addr_r=0x82000000
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_mmc; run run_fit;
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
mmcboot=mmc dev ${mmcdev}; setenv devnum ${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run l;
mmcdev=0
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; els;
mmcrootfstype=ext4 rootwait
netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdta}
netloadfdt=tftp ${fdtaddr} ${fdtfile}
netloadimage=tftp ${loadaddr} ${bootfile}
nfsopts=nolock
partitions=uuid_disk=${uuid_gpt_disk};name=bootloader,start=384K,size=1792K,uuid=${uuid_gpt_bootloader};name=rootfs,start=2688K,size=-,uui}
partitions_android=uuid_disk=${uuid_gpt_disk};name=xloader,start=128K,size=256K,uuid=${uuid_gpt_xloader};name=bootloader,size=2048K,uuid=$}
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rdaddr=0x88080000
rootpath=/export/rootfs
run_fit=bootm ${fit_loadaddr}#${fdtfile}${overlaystring}
scriptaddr=0x80000000
serial#=0b00f0133c4e08e2
soc=omap5
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial@48020000
stdin=serial@48020000
stdout=serial@48020000
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
usbtty=cdc_acm
vendor=ti
ver=U-Boot 2019.01 (Oct 16 2019 - 17:50:53 +0200)
vram=16M
Environment size: 7419/131067 bytes