This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Failed LSP1.20 patch 14



Dear sirs,

As I do not have the files I need (in the /lsp/ti-davinci/drivers/video/davinci directory), I attempted to update my system using the latest patches. I downloaded "REL_LSP_01_20_01_004.tar.gz" (which I assume to be the latest), follow the instructions (in patches/read.me) to the best of my ability, but if did not seam to work! This is what I got:

root@dell-desktop:/home/ioanprys/workdir/lsp/ti-davinci# sudo quilt push -a

Applying patch lsp_1_20_dm644x_pg_2_1_vid0_revert_field_inversion_fix_001.patch

patching file arch/arm/mach-davinci/id.c

Hunk #1 FAILED at 21.

Hunk #2 FAILED at 34.

2 out of 5 hunks FAILED -- rejects in file arch/arm/mach-davinci/id.c

patching file include/asm-arm/arch-davinci/cpu.h

Hunk #1 FAILED at 16.

Hunk #2 succeeded at 30 (offset -5 lines).

1 out of 2 hunks FAILED -- rejects in file include/asm-arm/arch-davinci/cpu.h

can't find file to patch at input line 105

Perhaps you used the wrong -p or --strip option?

The text leading up to this was:

--------------------------

|

|Index: Linux/drivers/media/video/davinci/davinci_display.c

|=========================================================================

|--- Linux-orig/drivers/media/video/davinci/davinci_display.c 2008-06-24 14:45:57.881792000 -0400

|+++ Linux/drivers/media/video/davinci/davinci_display.c 2008-06-24 15:00:02.215409000 -0400

--------------------------

No file to patch. Skipping patch.

1 out of 1 hunk ignored

can't find file to patch at input line 119

Perhaps you used the wrong -p or --strip option?

The text leading up to this was:

--------------------------

|

|Index: Linux/drivers/media/video/davinci/davinci_osd.c

|=====================================================================

|--- Linux-orig/drivers/media/video/davinci/davinci_osd.c 2008-06-24 14:45:57.900791000 -0400

|+++ Linux/drivers/media/video/davinci/davinci_osd.c 2008-06-24 15:00:02.269405000 -0400

--------------------------

No file to patch. Skipping patch.

2 out of 2 hunks ignored

can't find file to patch at input line 142

Perhaps you used the wrong -p or --strip option?

The text leading up to this was:

--------------------------

|

|Index: Linux/drivers/media/video/davinci/davinci_platform.c

|==========================================================================

|--- Linux-orig/drivers/media/video/davinci/davinci_platform.c 2008-06-24 14:45:57.912791000 -0400

|+++ Linux/drivers/media/video/davinci/davinci_platform.c 2008-06-24 15:00:02.298405000 -0400

--------------------------

No file to patch. Skipping patch.

1 out of 1 hunk ignored

can't find file to patch at input line 155

Perhaps you used the wrong -p or --strip option?

The text leading up to this was:

--------------------------

|Index: Linux/drivers/video/davinci/davincifb.c

|=============================================================

|--- Linux-orig/drivers/video/davinci/davincifb.c 2008-06-24 14:45:57.926799000 -0400

|+++ Linux/drivers/video/davinci/davincifb.c 2008-06-24 15:00:02.337410000 -0400

--------------------------

No file to patch. Skipping patch.

1 out of 1 hunk ignored

Patch lsp_1_20_dm644x_pg_2_1_vid0_revert_field_inversion_fix_001.patch does not apply (enforce with -f)

root@dell-desktop:/home/ioanprys/workdir/lsp/ti-davinci#

Can anyone help me?

Many thanks,

Ioan Prys

 

  • What base Linux kernel are you applying the patches to; ideally, this should be a Linux kernel that came with one of our DVSDKs.  Also, keep in mind that due to dependancies, it is a good rule of thumb to apply patches in sequence (unless you are very familiar with patches and know there are no dependencies).  Finally, keep in mind that depending on which base kernel you are working with, it may already have some or all of the patches you are trying to apply (DVSDK 1.30.00.41 has the directory you are referring to)

    Finally, I thought you may find the following wiki article useful

    http://wiki.davincidsp.com/index.php?title=Working_with_Linux_patches