This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

building CCS Project OMAP-L137 HelloDSP DSPLINK wiki

Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO

I am building CCS Project OMAP-L137 HelloDSP DSPLINK wiki
and get the following error in CCS 3.3
[Linking...] "C:\CCStudio_v3.3\bin\cl6x" -@"Debug.lkf"
<Linking>

 undefined first referenced                                                         
  symbol       in file                                                              
 --------- ----------------                                                         
 _main     C:/CCStudio_v3.3/bios_5_41_07_24/packages/ti/bios/lib/bios.a674<boot.o674>

error: unresolved symbols remain


Any Ideas on how to fix it.
Thanks

 

  • In your project, you must include in the source file that contains the main() function. And that main() function must be named exactly "main" and not "MyMain" or "Main", for example.

    Regards,
    RandyP

     

    If this answers your question, please click the  Verify Answer  button below. If not, please reply back with more information.

  • Thanks RandyP  Never mind my bad.  I missed a step in the add files to project section of the wiki.
    Had no main.c file in the project.... dah...
    Thanks
    Brian