This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EXEVM: Can TIDL model run on Tda2EG-17 with only 1 dsp 0 eve?

Part Number: TDA2EXEVM
Other Parts Discussed in Thread: TDA2EG-17, TDA2E

Hi,

We designed the tidl model to run smoothly on the TDA2x platform(2 dsp ,4 eve), and now we want the model to run on the TDA2EG-17 platform(750MHz 1DSP 0 eve ) due to the needs of the product.

We have verified that the running time is 13ms on TDA2x only using 4eve and 34ms on a single DSP(1000MHz), which is acceptable to us.

Even if the frequency is 750MHz.

However, we would like to confirm that on TDA2EG-17 platform, TIDL can be started without EVE?