Part Number: TMDSIDK574
I have TMDSIDK574 developement kit and i need to start processor after it powering without pressing any buttons. I found some document (www.ti.com/.../sliu011f.pdf Fig.4) which says me what I must to do with PMIC schematic. Moreover i must set bit AUTODEVON in 1 in PMU_CONFIG register. As I understood I must to use Static platform settings (or not?) and need to do next steps:
1. pin BOOT0 of TPS6590379ZWSR must be tied to VRTC_OUT(LDOVRTC_OUT).
2. pin GPIO_5 and GPIO_7 of TPS6590379ZWSR must be tied to VDD_RTC(LDO9_OUT).
3. relocate resistors R931 to R930 and R933 to 932.
If I wrong and you give me reference design or some notes to realise it i will be happy.