Other Parts Discussed in Thread: AM5716
The multiple QSPI-Flash for the AM5716's QSPI interface
Hello,
We are considering how to improve the access speed of QSPI, which causes are described in the related question.
Could you confirm the following questions?
1.Can we use multiple QSPI-Flash for the QSPI interface by the use of CTRL_CORE_CONTROL_IO_2.QSPI_MEMMAPPED_CS?
We want to use two 64M Byte QSPI-Flash instead of using one 128M Byte QSPI-Flash.
And we want to know the feasibility of that a QSPI-Flash is connected to CS0 and another Flash is connected to CS1.
2.Is this switching of CS supported by the Linux driver?
The SDK is PROCESSOR-SDK-LINUX-RT-AM57X and the version is v06_00_00_07.
3.If the answer of 1 and 2 is yes, can we switch the CS (accessing to each QSPI-Flash) dynamically?
Best Regards,
Nomo