This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Qt HDMI resolution issue

Part Number: AM5728

Hello,

I am using AM5728 of my custom board, and the martix gui also be displayed on HDMI with 1280x1024 when I connect usb mouse. Then I can run my QT application normally.  Without mouse, I also can run my QT app with parameter -platform eglfs, but resolution of HDMI is changed to 1024x768 so the window only can be showed a part. Please help me to modify the resolution of HDMI display when QT with eglfs. BTW, when I kill QT app, the resolution restore to 1280x1024 !

Thanks,

Best Regards,

Guan Qing