This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use EB tresos in TDA4 SW package

Hi,

I am trying to use the EB tresos. 

I already checked EB related guide via PSDKRA_RTOS\mcusw\mcal_drv\docs\drv_docs\mcusw_cfg_ug_top.html in TDA4_PSDKRA_RTOS v0.9.0.1 SW package.

And then, the steps such as."Copying the required MCAL plugins etc". is executed seeing the guide.

EB tresos generate many files acccording to selecting modules in output folder.

Currently, if EB tresos generate the files related to each module, I have to move the files to the related folder manually in TDA4_PSDKRA_RTOS v0.9.0.1 SW package.

Is there any method for automatically moving these files to the necessary positon in TDA4_PSDKRA_RTOS v0.9.0.1 SW package ?

Regards,

Alex Jung.

  • Hi Alex Jung,

    Yes, the generated files will have to be moved manually.

    Please note that demo & example applications in MCUSW might require an update to work with update/modified configurations.

    Regards, Sujith