Part Number: PROCESSOR-SDK-DRA8X
Hello,
we want to use USB1 port in Host Mode only.
Should we add a pulldown or pullup to USB1_VBUS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-DRA8X
Hello,
we want to use USB1 port in Host Mode only.
Should we add a pulldown or pullup to USB1_VBUS?
Hi,
USBx_VBUS must be connected to VBUS.
Note that this pin is a 3.3-V pin and the 5-V VBUS must be applied via an external divider of few 10s of kOhms.
Regards,
Stan
Hi,
there is no VBUS - only USB1_DP/DM will be connected to an external hub via a cable. This is part of a debug toolchain.
Regards,
Ron
Would be good VBUS (sense) to be connected to DRVVBUS. Make sure the DRVVBUS pin chosen (there are several possible) is powered by 3.3V.
I guess, it is also possible to hardwire VBUS to a 3.3V IO supply via a pullup.