This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: SPI loopback

Part Number: PROCESSOR-SDK-AM335X


Hi,

I am using EVMSKAm335x processor kit and processor sdk rtos. As no slave is connected to SPI in starter kit of AM3358x so can we check SPI through loopback?

How can I configure SPI for loopback? I didn't get any bit in any register to configure for loopback.

Regards

Gaurav

  • Hi Gaurav,

    I'm also unable to locate a hardware loopback mode for the McSPI in the TRM.

    I see a McSPI loopback example in AM335x PRSDK 6.0.0.7 here: pdk_am335x_1_0_15\packages\ti\drv\spi\example\mcspiLoopbackApp The source code for this example is here: pdk_am335x_1_0_15\packages\ti\drv\spi\example\mcspiLoopbackApp\src\mcspiLoopbackApp.c. Looking inside this file, I observe the following comments:

    * \brief This file contains the application which demonstrates McSPI loopback
    * which transfers some data pattern from data I/O signal & receives
    * the data from same data I/O signal.

    /* Loopback mode is not available for MCSPI. To test Loopback on McSPI,
    * Receive Bit is enabled on both Tx and Rx pins of McSPI
    */

    This directory contains the AM335x platform-specific files for this example: pdk_am335x_1_0_15\packages\ti\drv\spi\example\mcspiLoopbackApp\am335x\armv7\bios. In this directory, I only see project text files for evmAM335x and iceAMIC110. However, I think it should be possible to add a project file for skAM335x:

    1. Copy mcspi_loopback_arm_evmAM335x.cfg to a new file in the same directory named mcspi_loopback_arm_skAM335x.cfg

    2. Update settings in mcspi_loopback_arm_skAM335x.cfg:

    • Board.Settings.boardName = "skAM335x";

    2. Copy MCSPI_Loopback_evmAM335x_armExampleProject.txt to a new file in the same directory named MCSPI_Loopback_skAM335x_armExampleProject.txt.

    3. Update settings in MCSPI_Loopback_skAM335x_armExampleProject.txt:

    • Update link for cfg file: set -ccs.linkFile to mcspi_loopback_arm_skAM335x.cfg
    • Update compiler options: update -ccs.setCompilerOptions for relevant options found in another SK example
      •  SK example: pdk_am335x_1_0_15\packages\ti\drv\i2c\example\eeprom_read\am335x\armv7\bios\I2C_Example_skAM335x_armExampleProject.txt
      • Example of relevant option: -DskAM335x

    4. Create new SK project: pdkprojectcreate AM335x skAM335x little spi example arm

    Regards,
    Frank

  • Hi Gaurav,

    I verified the above approach works for creating a new SK CCS project for the McSPI loopback example.

    The CCS project is placed here after executing pdkprojectcreate: pdk_am335x_1_0_15\packages\MyExampleProjects. I verified I was able to import the CCS project and that the project builds. Unfortunately I don't currently have access to an SK to verify correct operation of the build.

    I've attached the files below. You may still need to modify some settings for the behavior you observe when executing the program on the SK.

    Regards,
    Frank

    mcspi_loopback_arm_skAM335x.cfg

    -ccs.linkFile "PDK_INSTALL_PATH/ti/drv/spi/example/mcspiLoopbackApp/src/mcspiLoopbackApp.c"
    -ccs.linkFile "PDK_INSTALL_PATH/ti/drv/spi/example/mcspiLoopbackApp/am335x/armv7/bios/mcspi_loopback_arm_skAM335x.cfg" 
    -ccs.setCompilerOptions "-c -mcpu=cortex-a8 -mtune=cortex-a8 -march=armv7-a -marm -mfloat-abi=hard -DUART_V1 -DSOC_AM335x -DBUILDCFG_MOD_SPI -DskAM335x -g -gstrict-dwarf -gdwarf-3 -finstrument-functions -Wall -MMD -MP -I${PDK_INSTALL_PATH}/ti/drv/spi -I${PDK_INSTALL_PATH} -I${PDK_INSTALL_PATH}/ti/starterware/board/am335x -I${PDK_INSTALL_PATH}/ti/starterware/include/am335x -I${PDK_INSTALL_PATH}/ti/starterware/include -I${EDMA3LLD_BIOS6_INSTALLDIR}/packages "  -rtsc.enableRtsc
    -ccs.setLinkerOptions " -lgcc -lrdimon -lm -lnosys -nostartfiles -static -Wl,--gc-sections "
    
    

  • Hi,

    I wrote a SPI program for transmit and receive. I have connected D0 and D1 line physically, but SPI is not working. Please check the flow of program, if any configuration missed please let me know. I am attaching mcspi.c and mcspi.h file for declaration and functions definitions.

    I am configuring SPI in 3 pin mode.

    unsigned int a=0;

    SPI0ModuleClkConfig();

    McSPIPinMuxSetup();

    /* Reset the McSPI instance.*/
    McSPIReset(SOC_SPI_0_REGS);

    /* Enable chip select pin.*/
    McSPICSDisable(SOC_SPI_0_REGS);

    /* Enable master mode of operation.*/
    McSPIMasterModeEnable(SOC_SPI_0_REGS);

    //Perform the necessary configuration for master mode.
    McSPIMasterModeConfig(SOC_SPI_0_REGS, MCSPI_SINGLE_CH,
    MCSPI_TX_RX_MODE, MCSPI_DATA_LINE_COMM_MODE_0,
    chNum);

    //Configure the McSPI bus clock depending on clock mode.
    McSPIClkConfig(SOC_SPI_0_REGS, 48000000, 24000000, chNum,
    MCSPI_CLK_MODE_0);

    /* Configure the word length.*/
    McSPIWordLengthSet(SOC_SPI_0_REGS, MCSPI_WORD_LENGTH(8), chNum);

    /* Set polarity of SPIEN to low.*/
    McSPICSPolarityConfig(SOC_SPI_0_REGS, MCSPI_CS_POL_LOW, chNum);

    /* SPIEN line is forced to low state.*/
    McSPICSAssert(SOC_SPI_0_REGS, chNum);

    /* Enable the McSPI channel for communication.*/
    McSPIChannelEnable(SOC_SPI_0_REGS, chNum);

    /* Force SPIEN line to the inactive state.*/
    McSPICSDeAssert(SOC_SPI_0_REGS, chNum);

    while(1)
    {
    //while(!(HWREG(SOC_SPI_0_REGS + MCSPI_CHSTAT(0))&(1<<1)));
    McSPITransmitData(SPI_BASE_ADD,8,MCSPI_CHANNEL_0);

    ConsoleUtilsPrintf("a1=%d\n",a);

    //while(!(HWREG(SOC_SPI_0_REGS + MCSPI_CHSTAT(0))&(1<<0)));
    a=McSPIReceiveData(SPI_BASE_ADD,MCSPI_CHANNEL_0);

    ConsoleUtilsPrintf("a=%d",a);
    }

    /* Disable the McSPI channel.*/
    McSPIChannelDisable(SOC_SPI_0_REGS, chNum);

    Regards

    Gaurav

    /**
    *
    *  \file mcspi.c
    *
    *  \brief McSPI device abstraction layer APIs
    **/
    
    /*
    * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/
    */
    /*
    *  Redistribution and use in source and binary forms, with or without
    *  modification, are permitted provided that the following conditions
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the
    *    documentation and/or other materials provided with the
    *    distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    */
    
    #include "mcspi.h"
    #include "hw_control_AM335x.h"
    #include "evmskAM335x.h"
    #include "soc_AM335x.h"
    #include "hw_cm_wkup.h"
    #include "hw_cm_per.h"
    #include "hw_types.h"
    
    /*******************************************************************************
    *                       INTERNAL MACRO DEFINITIONS
    *******************************************************************************/
    #define MCSPI_CH_NUM_0        (0u)
    #define MCSPI_CLKD_MASK       (0xF)
    
    /*******************************************************************************
    *                        API FUNCTION DEFINITIONS
    *******************************************************************************/
    
    /**
    * \brief  This API will configure the clkD and extClk fields to generate 
    *         required spi clock depending on the type of granularity. It will 
    *         also set the phase and polarity of spiClk by the clkMode field.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  spiInClk       Clock frequency given to the McSPI module.
    * \param  spiOutClk      Clock frequency on the McSPI bus.
    * \param  chNum          Channel number of the McSPI instance used. 
    * \param  clkMode        Clock mode used.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    *         'clkMode' can take the following values.\n
    *         MCSPI_CLK_MODE_n - McSPI clock mode n.\n
    *
    *         For clkMode 0 <= n <= 3.\n
    *
    * \return none.
    *
    * \note:  1) clkMode depends on phase and polarity of McSPI clock.\n
    *         2) To pass the desired value for clkMode please refer the 
    *            McSPI_CH(i)CONF register.\n
    *         3) Please understand the polarity and phase of the slave device 
    *            connected and accordingly set the clkMode.\n
    *         4) McSPIClkConfig does not have any significance in slave mode 
    *            because the clock signal required for communication is generated 
    *            by the master device.
    **/
    void McSPIClkConfig(unsigned int baseAdd, unsigned int spiInClk, 
                        unsigned int spiOutClk, unsigned int chNum, 
                        unsigned int clkMode)
    {
        unsigned int fRatio = 0;    
        unsigned int extClk = 0;
        unsigned int clkD = 0;
    
        /* Calculate the value of fRatio. */
        fRatio = (spiInClk / spiOutClk);
     
        /* If fRatio is not a power of 2, set granularity of 1 clock cycle */
        if(0 != (fRatio & (fRatio - 1))) 
        {
            /* Set the clock granularity to 1 clock cycle.*/
            HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= MCSPI_CH0CONF_CLKG;
    
            /* Calculate the ratios clkD and extClk based on fClk */
            extClk = (fRatio - 1) >> 4;
            clkD = (fRatio - 1) & MCSPI_CLKD_MASK;
    
            /*Clear the extClk field of MCSPI_CHCTRL register.*/
            HWREG(baseAdd + MCSPI_CHCTRL(chNum)) &= ~MCSPI_CH0CTRL_EXTCLK;
    
            /* Set the extClk field of MCSPI_CHCTRL register.*/
            HWREG(baseAdd + MCSPI_CHCTRL(chNum)) |= (extClk << 
                                                     MCSPI_CH0CTRL_EXTCLK_SHIFT);
        }
        else
        {
            /* Clock granularity of power of 2.*/
            HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_CLKG;
    
            while(1 != fRatio)
            {
                fRatio /= 2;
                clkD++;
            }
        }
    
        /*Clearing the clkD field of MCSPI_CHCONF register.*/
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_CLKD;
    
        /* Configure the clkD field of MCSPI_CHCONF register.*/
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (clkD << MCSPI_CH0CONF_CLKD_SHIFT);
             
        /*Clearing the clkMode field of MCSPI_CHCONF register.*/
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~(MCSPI_CH0CONF_PHA | 
                                                   MCSPI_CH0CONF_POL);
    
        /* Configure the clkMode of MCSPI_CHCONF register.*/
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (clkMode & (MCSPI_CH0CONF_PHA | 
                                                             MCSPI_CH0CONF_POL));
    }
    
    /**
    * \brief  This API will configure the length of McSPI word used for 
    *         communication. 
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  wordLength     Length of a data word used for McSPI communication.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'wordLength' can take the following values.\n
    *          MCSPI_WORD_LENGTH(n)  - McSPI word length is n bits long.\n
    *
    *          For wordLength 4 <= n <= 32.\n
    *
    *          'chNum' can take the following values.\n
    *          MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *          For chNum n can vary from 0-3.\n
    *
    * \return none.
    *
    * \note:  wordLength can vary from 4-32 bits length. To program the
    *         required value of wordLength please refer the MCSPI_CH(i)CONF 
    *         register.\n
    **/
    void McSPIWordLengthSet(unsigned int baseAdd, unsigned int wordLength,
                            unsigned int chNum)
    {
        /*Clearing the wordLength field of MCSPI_CHCONF register.*/
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_WL;
    
        /* Setting the wordlength field. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (wordLength & MCSPI_CH0CONF_WL);
    }
    
    /**
    * \brief  This API will enable the chip select pin.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    *
    * \return none.
    *
    * \note:  Modification of CS polarity, SPI clock phase and polarity 
              is not allowed when CS is enabled.
    **/
    void McSPICSEnable(unsigned int baseAdd)
    {
        /* CLear PIN34 of MCSPI_MODULCTRL register. */
        HWREG(baseAdd + MCSPI_MODULCTRL) &= ~MCSPI_MODULCTRL_PIN34;                 
    }
    
    /**
    * \brief  This API will disable the chip select pin.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    *
    * \return none.
    **/
    void McSPICSDisable(unsigned int baseAdd)
    {
        /* Set PIN34 of MCSPI_MODULCTRL register.*/
        HWREG(baseAdd + MCSPI_MODULCTRL) |= MCSPI_MODULCTRL_PIN34;             
    }
    
    /**
    * \brief  This API will configure the chip select polarity.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  spiEnPol       Polarity of CS line.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *        'spiEnPol' can take the following values.\n
    *         MCSPI_CS_POL_HIGH - SPIEN pin is held high during the active state.\n
    *         MCSPI_CS_POL_LOW - SPIEN pin is held low during the active state.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPICSPolarityConfig(unsigned int baseAdd, unsigned int spiEnPol,
                               unsigned int chNum) 
    {
        /* Clear the EPOL field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_EPOL;
    
        /* Set the EPOL field with the user sent value. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (spiEnPol & MCSPI_CH0CONF_EPOL);
    }
    
    /**
    * \brief  This API will configure the chip select time control.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  csTimeControl  Chip Select time control.
    * \param  chNum          Channel number of the McSPI instance used.
    *
    *         'csTimeControl' can take the following values.\n
    *         MCSPI_CS_TCS_nPNT5_CLK - n.5 Clock cycles.\n
    *
    *         For csTimeControl 0 <= n <= 3.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPICSTimeControlSet(unsigned int baseAdd, unsigned int csTimeControl,
                               unsigned int chNum)
    {
        /* Clear the TCS field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_TCS0;
    
        /* Set the TCS field with the user sent value. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= ((csTimeControl <<
                                                  MCSPI_CH0CONF_TCS0_SHIFT) &
                                                  MCSPI_CH0CONF_TCS0);
    }
    
    /**
    * \brief  This API will activate the chip select line.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPICSAssert(unsigned int baseAdd, unsigned int chNum)
    {
        /* Set the FORCE bit of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (MCSPI_CH0CONF_FORCE);
    }
    
    /**
    * \brief  This API will deactivate the chip select line.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPICSDeAssert(unsigned int baseAdd, unsigned int chNum)
    {
        /* Clear the FORCE bit of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~(MCSPI_CH0CONF_FORCE);
    }
    
    /**
    * \brief  This API will enable start bit.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n  
    *
    * \return none.
    **/
    void McSPIStartBitEnable(unsigned int baseAdd, unsigned int chNum)
    {
        /* Set the SBE bit of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= MCSPI_CH0CONF_SBE; 
    }
    
    /**
    * \brief  This API will configure the polarity of start bit.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  startBitPol    Polarity of start bit.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'startBitPol' can take the following values.\n
    *         MCSPI_START_BIT_POL_LOW  - Polarity of start bit is held low
    *                                    during transmission.\n
    *         MCSPI_START_BIT_POL_HIGH - Polarity of start bit is held high
    *                                    during transmission.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPIStartBitPolarityConfig(unsigned int baseAdd, unsigned int startBitPol, 
                                     unsigned int chNum)
    {
        /* Clear the SBE field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_SBPOL;     
       
        /* Set the user sent value */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (startBitPol & 
                                                  MCSPI_CH0CONF_SBPOL);
    }
    
    /**
    * \brief  This API will disable the start bit mode of McSPI peripheral.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPIStartBitDisable(unsigned int baseAdd, unsigned int chNum)
    {
        /* Clear the SBE field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_SBE; 
    }
    
    /**
    * \brief  This API will enable the McSPI controller in master mode.  
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    *
    * \return none.
    **/
    void McSPIMasterModeEnable(unsigned int baseAdd)
    {
        /* Clear the MS field of MCSPI_MODULCTRL register. */
        HWREG(baseAdd + MCSPI_MODULCTRL) &= ~MCSPI_MODULCTRL_MS; 
    }
    
    /**
    * \brief  This API will enable the McSPI controller in master mode and 
    *         configure other parameters required for master mode.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  channelMode    Single/Multi channel.
    * \param  trMode         Transmit/Receive mode used in master 
    *                        configuration.
    * \param  pinMode        Interface mode and pin assignment.                                
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'channelMode' can take the following values.\n
    *         MCSPI_SINGLE_CH - Single channel mode is used.\n
    *         MCSPI_MULTI_CH  - Multi channel mode is used.\n
    *
    *         'trMode' can take the following values.\n
    *         MCSPI_TX_RX_MODE   - Enable McSPI in TX and RX modes.\n
    *         MCSPI_RX_ONLY_MODE - Enable McSPI only in RX mode.\n
    *         MCSPI_TX_ONLY_MODE - Enable McSPI only in TX mode.\n
    *
    *         'pinMode' can take the following values.\n
    *         MCSPI_DATA_LINE_COMM_MODE_n - Mode n configuration for SPIDAT[1:0].\n
    *
    *         For pinMode 0 <= n <= 7.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return 'retVal' which states if the combination of trMode and pinMode chosen 
    *          by the user is supported for communication on SPIDAT[1:0] pins.\n
    *          TRUE  - Communication supported by SPIDAT[1:0].\n
    *          FALSE - Communication not supported by SPIDAT[1:0].\n
    *
    * \note   Please refer the description about IS,DPE1,DPE0 and TRM bits for 
    *         proper configuration of SPIDAT[1:0].\n
    **/
    unsigned int McSPIMasterModeConfig(unsigned int baseAdd,
                                       unsigned int channelMode, 
                                       unsigned int trMode, 
                                       unsigned int pinMode,
                                       unsigned int chNum)
    {
        unsigned int retVal = FALSE;
        
        HWREG(baseAdd + MCSPI_SYST) = (0<<9)|(1<<8)|(0<<5)|(1<<4);//|(0<<10)|(0<<0);
    
        /* Clear the MS field of MCSPI_MODULCTRL register. */
        HWREG(baseAdd + MCSPI_MODULCTRL) &= ~MCSPI_MODULCTRL_SINGLE;
    
        /* Set the MS field with the user sent value. */
        HWREG(baseAdd + MCSPI_MODULCTRL) |= (channelMode & MCSPI_MODULCTRL_SINGLE);
    
        /* Clear the TRM field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_TRM;
    
        /* Set the TRM field with the user sent value. */
        //HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= //(trMode & MCSPI_CH0CONF_TRM);
    
        if(((MCSPI_TX_RX_MODE == trMode) && 
           (MCSPI_DATA_LINE_COMM_MODE_3 == pinMode)) || 
           ((MCSPI_TX_ONLY_MODE == trMode) && 
           (MCSPI_DATA_LINE_COMM_MODE_3 == pinMode)) || 
           ((MCSPI_TX_RX_MODE == trMode) && 
           (MCSPI_DATA_LINE_COMM_MODE_7 == pinMode)) || 
           ((MCSPI_TX_ONLY_MODE == trMode) && 
           (MCSPI_DATA_LINE_COMM_MODE_7 == pinMode)))
        {
            retVal = FALSE;
        }
        else 
        {
            /* Clear the IS, DPE0, DPE1 fields of MCSPI_CHCONF register. */
            HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~(MCSPI_CH0CONF_IS | 
                                                       MCSPI_CH0CONF_DPE1 | 
                                                       MCSPI_CH0CONF_DPE0);
      
            /* Set the IS, DPE0, DPE1 fields with the user sent values. */
            HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (pinMode & (MCSPI_CH0CONF_IS |
                                                                MCSPI_CH0CONF_DPE1 | 
                                                                MCSPI_CH0CONF_DPE0));
    
            retVal = TRUE;
        }
    
        return retVal;
    }
    
    /**
    * \brief  This API will enable the channel of McSPI controller.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *      'chNum' can take the following values.\n
    *      MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *      For chNum 0 <= n <= 3.\n
    *
    * \return none.
    *
    * \note:  Please ensure to enable only channel 0 in slave mode.\n
    *         Channels other than 0 are not valid in slave mode.
    **/
    void McSPIChannelEnable(unsigned int baseAdd, unsigned int chNum)
    {
        /* Set the EN field of MCSPI_CHCTRL register. */
        HWREG(baseAdd + MCSPI_CHCTRL(chNum)) |= MCSPI_CH0CTRL_EN_ACTIVE;                        
    }
    
    /**
    * \brief  This API will disable the channel of McSPI controller.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPIChannelDisable(unsigned int baseAdd, unsigned int chNum)
    {
        /* Clear the EN field of MCSPI_CHCTRL register. */
        HWREG(baseAdd + MCSPI_CHCTRL(chNum)) &= ~MCSPI_CH0CTRL_EN_ACTIVE;                   
    }
    
    /**
    * \brief  This API will reset the McSPI peripheral.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    *
    * \return none.
    **/
    void McSPIReset(unsigned int baseAdd)
    {
        /* Set the SOFTRESET field of MCSPI_SYSCONFIG register. */
        HWREG(baseAdd + MCSPI_SYSCONFIG) |= MCSPI_SYSCONFIG_SOFTRESET; 
        
        /* Stay in the loop until reset is done. */
        while(!(MCSPI_SYSSTATUS_RESETDONE_COMPLETED & 
                HWREG(baseAdd + MCSPI_SYSSTATUS))); 
    }
    
    /**
    * \brief  This API will enable the McSPI turbo mode of operation. 
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    *
    * \note   
    **/
    void McSPITurboModeEnable(unsigned int baseAdd, unsigned int chNum)
    {
        /* Set the TURBO field on MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= MCSPI_CH0CONF_TURBO; 
    }
    
    /**
    * \brief  This API will disable the McSPI turbo mode of operation. 
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum 0 <= n <= 3.\n
    *
    * \return none.
    **/
    void McSPITurboModeDisable(unsigned int baseAdd, unsigned int chNum)
    {
        /* Clear the TURBO field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_TURBO;
    }
    
    /**
    * \brief  This API will enable/disable the Tx FIFOs of McSPI peripheral.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  txFifo         FIFO used for transmit mode.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'txFifo' can take the following values.\n
    *         MCSPI_TX_FIFO_ENABLE  - Enables the transmitter FIFO of McSPI.\n
    *         MCSPI_TX_FIFO_DISABLE - Disables the transmitter FIFO of McSPI.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    *
    * \note:  Enabling FIFO is restricted to only 1 channel.
    **/
    void McSPITxFIFOConfig(unsigned int baseAdd, unsigned int txFifo, 
                           unsigned int chNum)
    {
        /* Clear the FFEW field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_FFEW;
    
        /* Set the FFEW field with user sent value. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (txFifo & MCSPI_CH0CONF_FFEW); 
    }
    
    /**
    * \brief  This API will enable/disable the Rx FIFOs of McSPI peripheral.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  rxFifo         FIFO used for receive mode.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'rxFifo' can take the following values.\n
    *         MCSPI_RX_FIFO_ENABLE - Enables the receiver FIFO of McSPI.\n
    *         MCSPI_RX_FIFO_DISABLE - Disables the receiver FIFO of McSPI.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    *
    * \note:  Enabling FIFO is restricted to only 1 channel.
    **/
    void McSPIRxFIFOConfig(unsigned int baseAdd, unsigned int rxFifo, 
                           unsigned int chNum)
    {
        /* Clear the FFER field of MCSPI_CHCONF register. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~MCSPI_CH0CONF_FFER;
    
        /* Set the FFER field with the user sent value. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (rxFifo & MCSPI_CH0CONF_FFER);
    }
    
    /**
    * \brief  This API will set the transfer levels used by FIFO depending on 
    *         the various McSPI transmit/receive modes. 
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  afl            Buffer almost full value.
    * \param  ael            Buffer almost empty value.
    * \param  trMode         Transmit/Receive modes used.\n 
    *
    *         'trMode' can take the following values.\n
    *         MCSPI_TX_RX_MODE   - Enable McSPI in TX and RX modes.\n
    *         MCSPI_RX_ONLY_MODE - Enable McSPI only in RX mode.\n
    *         MCSPI_TX_ONLY_MODE - Enable McSPI only in TX mode.\n
    *      
    * \return none.
    *
    * \note   Values for afl and ael will have varying values depending on
    *         trMode. If trMode is MCSPI_TX_RX_MODE then afl and ael can take 
    *         values ranging from 0-19. If trMode is MCSPI_RX_ONLY_MODE/
    *         MCSPI_TX_ONLY_MODE then afl and ael can take values from 0-39.\n
    *
    *         While configuring mode of operation using trMode please ensure the 
    *         same value of trMode is used while using API's McSPIMasterModeConfig
    *         and McSPISlaveModeConfig. Mismatch while using trMode for different 
    *         APIs can result in unpredictable behaviour.\n 
    *
    *         For 'ael' and 'afl' please send level values for both of the fields
    *         and do not send the value which has to be written into the register 
    *         for the corresponding level value.
    *         For e.g. if 'ael' or 'afl' has to be 1 byte, then pass the parameter 
    *         'ael' or 'afl' as 1 and not 0 because the value which has to be 
    *         written into register is manipulated inside the driver itself.\n
    **/
    void McSPIFIFOTrigLvlSet(unsigned int baseAdd, unsigned char afl, 
                             unsigned char ael, unsigned int trMode)
    {
        if(MCSPI_TX_RX_MODE == trMode)
        {
            /* Clear the AFL and AEL fields of MCSPI_XFERLEVEL register. */
            HWREG(baseAdd + MCSPI_XFERLEVEL) &= ~(MCSPI_XFERLEVEL_AFL | 
                                                  MCSPI_XFERLEVEL_AEL);
    
            /* Set the AFL and AEL fields with the user sent value. */
            HWREG(baseAdd + MCSPI_XFERLEVEL) |= ((((afl-1) << 
                                                 MCSPI_XFERLEVEL_AFL_SHIFT) & 
                                                 MCSPI_XFERLEVEL_AFL) | 
                                                 ((ael - 1) & MCSPI_XFERLEVEL_AEL));
        }
        else if(MCSPI_TX_ONLY_MODE == trMode)
        {
            /* Clear the AEL field of MCSPI_XFERLEVEL register. */
            HWREG(baseAdd + MCSPI_XFERLEVEL) &= ~MCSPI_XFERLEVEL_AEL;
    
            /* Set the AEL field with the user sent value. */
            HWREG(baseAdd + MCSPI_XFERLEVEL) |= ((ael - 1) & MCSPI_XFERLEVEL_AEL);
        }
        else if(MCSPI_RX_ONLY_MODE == trMode)
        {
            /* Clear the AFL field of MCSPI_XFERLEVEL register. */
            HWREG(baseAdd + MCSPI_XFERLEVEL) &= ~MCSPI_XFERLEVEL_AFL;
    
            /* Set the AFL field with the user sent value. */
            HWREG(baseAdd + MCSPI_XFERLEVEL) |= (((afl - 1) << 
                                                   MCSPI_XFERLEVEL_AFL_SHIFT) & 
                                                   MCSPI_XFERLEVEL_AFL);
        }
        else
        {
    
        }
    }
    
    /**
    * \brief  This API will set the McSPI word counter value. 
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  wCnt           Word count.
    *
    * \return none.
    **/
    void McSPIWordCountSet(unsigned int baseAdd, unsigned short wCnt)
    {
        /* Clear the WCNT field of MCSPI_XFERLEVEL register. */
        HWREG(baseAdd + MCSPI_XFERLEVEL) &= ~MCSPI_XFERLEVEL_WCNT;
    
        /* Set the WCNT field with the user sent value. */
        HWREG(baseAdd + MCSPI_XFERLEVEL) |= (wCnt << MCSPI_XFERLEVEL_WCNT_SHIFT);
    }
    
    /**
    * \brief  This API will enable the DMA read/write events of McSPI.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  dmaFlags       Variable used to enable DMA mode for 
    *                        Rx/Tx events.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'dmaFlags' can take the following values.\n
    *         MCSPI_DMA_RX_EVENT  - To enable DMA mode for Rx events.\n
    *         MCSPI_DMA_TX_EVENT  - To enable DMA mode for Tx events.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    **/
    void McSPIDMAEnable(unsigned int baseAdd, unsigned int dmaFlags,
                        unsigned int chNum)
    {
        /* Enable the DMA events. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) |= (dmaFlags & (MCSPI_CH0CONF_DMAR |
                                                              MCSPI_CH0CONF_DMAW)); 
    }
    
    /**
    * \brief  This API will disable the DMA read/write events of McSPI.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  dmaFlags       Variable used to disable DMA mode for
    *                        Rx/Tx events.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'dmaFlags' can take the following values.\n
    *         MCSPI_DMA_RX_EVENT - To disable DMA mode for Rx events.\n
    *         MCSPI_DMA_TX_EVENT - To disable DMA mode for Tx events.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    **/
    void McSPIDMADisable(unsigned int baseAdd, unsigned int dmaFlags,
                         unsigned int chNum)
    {
        /* Disable the DMA events. */
        HWREG(baseAdd + MCSPI_CHCONF(chNum)) &= ~(dmaFlags & (MCSPI_CH0CONF_DMAR | 
                                                               MCSPI_CH0CONF_DMAW));
    }
    
    /**
    * \brief  This API will enable the McSPI Interrupts.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  intFlags       Represents the various interrupts to be enabled.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'intFlags' can take the following values.\n
    *         MCSPI_INT_TX_EMPTY(chan) - Transmitter register empty interrupt.\n
    *         MCSPI_INT_TX_UNDERFLOW(chan) - Transmitter register underflow 
    *                                        interrupt.\n
    *         MCSPI_INT_RX_FULL(chan) - Receiver register full interrupt.\n
    *         MCSPI_INT_RX0_OVERFLOW - Receiver register 0 overflow interrupt.\n
    *         MCSPI_INT_EOWKE - End of word count interrupt.\n
    *
    *         'chan' stands for channel number. 
    *         Please specify the proper channel number while passing the macros.
    *         0 <= chan <= 3 \n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    *
    * \note   Please ensure the proper channel number is passed while using the 
    *         macros.
    **/
    void McSPIIntEnable(unsigned int baseAdd, unsigned int intFlags)
    {
        /* Enable the Interrupts. */
        HWREG(baseAdd + MCSPI_IRQENABLE) |= intFlags;
    }
    
    /**
    * \brief  This API will disable the McSPI Interrupts.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  intFlags       Represents the various interrupts to be disabled.
    *
    *         'intFlags' can take the following values.\n
    *         MCSPI_INT_TX_EMPTY(chan) - Transmitter register empty interrupt.\n
    *         MCSPI_INT_TX_UNDERFLOW(chan) - Transmitter register underflow 
    *                                        interrupt.\n
    *         MCSPI_INT_RX_FULL(chan) - Receiver register full interrupt.\n
    *         MCSPI_INT_RX0_OVERFLOW - Receiver register 0 overflow interrupt.\n
    *         MCSPI_INT_EOWKE - End of word count interrupt.\n
    *
    *         'chan' stands for channel number.
    *         Please specify the proper channel number while passing the macros.
    *         0 <= chan <= 3 \n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    *
    * \note   Please ensure the proper channel number is passed while using the
    *         macros.
    **/
    void McSPIIntDisable(unsigned int baseAdd, unsigned int intFlags)
    {
        /* Disable the interrupts. */
        HWREG(baseAdd + MCSPI_IRQENABLE) &= ~intFlags;
    }
    
    /**
    * \brief  This API will set initial delay for first transfer from McSPI 
    *         peripheral.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  initDelay      Delay used for first transfer.\n
    *
    *         'initDelay' can take the following values.\n
    *         MCSPI_INITDLY_0  - No delay for first transfer.\n
    *         MCSPI_INITDLY_4  - Delay of 4 SPI Clock.\n
    *         MCSPI_INITDLY_8  - Delay of 8 SPI Clock.\n
    *         MCSPI_INITDLY_16 - Delay of 16 SPI Clock.\n
    *         MCSPI_INITDLY_32 - Delay of 32 SPI Clock.\n
    *
    * \return none.
    *
    * \note:  Please note that this option is available only in single master mode.
    **/
    void McSPIInitDelayConfig(unsigned int baseAdd, unsigned int initDelay)
    {
        /* Clear the INITDLY field of MCSPI_MODULCTRL register. */
        HWREG(baseAdd + MCSPI_MODULCTRL) &= ~MCSPI_MODULCTRL_INITDLY;
    
        /* Set the INITDLY field with the user sent value. */
        HWREG(baseAdd + MCSPI_MODULCTRL) |= (initDelay & MCSPI_MODULCTRL_INITDLY);
    }
    
    /**
    * \brief  This API will put the data on to the McSPI Channel 
    *         transmit register.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  txData         32 bit data sent by the user which is put on 
    *                        to the MCSPI_TX register.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    **/
    void McSPITransmitData(unsigned int baseAdd, unsigned int txData,
                           unsigned int chNum)
    {
        while(!(HWREG(SOC_SPI_0_REGS + MCSPI_CHSTAT(0))&(1<<1)));
        /* Load the MCSPI_TX register with the data to be transmitted */
        HWREG(baseAdd + MCSPI_TX(chNum)) = txData;
    }
    
    /**
    * \brief  This API will return the data present in the MCSPI_RX register.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel number of the McSPI instance used.
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return This API will return the data received in the MCSPI_RX register.
    **/
    unsigned int McSPIReceiveData(unsigned int baseAdd, unsigned int chNum)
    {
        while(!(HWREG(SOC_SPI_0_REGS + MCSPI_CHSTAT(0))&(1<<0)));
        /* Return the data present in the MCSPI_RX register. */
        return(HWREG(baseAdd + MCSPI_RX(chNum)));
    }
    
    /**
    * \brief  This API will return the status of the McSPI peripheral interrupts.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    *
    * \return This API will return the status of the McSPI peripheral interrupts.
    *         User can use the following macros to check the status \n
    *         MCSPI_INT_TX_EMPTY(chan) - Transmitter register empty for channel n \n
    *         MCSPI_INT_TX_UNDERFLOW(chan) - Transmitter register underflow for 
    *                                        channel n \n
    *         MCSPI_INT_RX_FULL(chan) - Receiver register full for channel n \n
    *         MCSPI_INT_RX0_OVERFLOW - Receiver register overflow for channel 0 \n
    *         MCSPI_INT_EOWKE - End of word count interrupt \n
    *         where 0 <= chan <= 3
    *
    **/
    unsigned int McSPIIntStatusGet(unsigned int baseAdd)
    {
        /* Return the interrupt status present in the MCSPI_IRQSTATUS register. */
        return(HWREG(baseAdd + MCSPI_IRQSTATUS));
    } 
    
    /**
    * \brief  This API will clear the status of McSPI Interrupts.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  intFlags       Represents the various interrupts to be cleared.
    * \param  chNum          Channel number of the McSPI instance used.\n
    *
    *         intFlags can take the following values.\n
    *         MCSPI_INT_TX_EMPTY(chan) - Transmitter register empty interrupt.\n
    *         MCSPI_INT_TX_UNDERFLOW(chan) - Transmitter register underflow 
    *                                        interrupt.\n
    *         MCSPI_INT_RX_FULL(chan) - Receiver register full interrupt.\n
    *         MCSPI_INT_RX0_OVERFLOW - Receiver register 0 overflow interrupt.\n
    *         MCSPI_INT_EOW - End of word count interrupt.\n
    *
    *         'chan' stands for channel number. Please ensure proper channel 
    *         number is used while passing the macros.
    *         0 <= chan <= 3 \n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    *         For chNum n can range from 0-3.\n
    *
    * \return none.
    *
    * \note   Please ensure the proper channel number is used while passing the 
    *         macros passed.\n
    **/
    void McSPIIntStatusClear(unsigned int baseAdd, unsigned int intFlags)
    {
        /* Clear the SSB bit in the MCSPI_SYST register. */
        HWREG(baseAdd + MCSPI_SYST) &= ~MCSPI_SET_STATUS_BIT;        
            
        /* Clear the interrupt status. */
        HWREG(baseAdd + MCSPI_IRQSTATUS) = intFlags;
    }
    
    /**
    * \brief  This API will return the status of the McSPI channel currently in 
    *         use.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  chNum          Channel used for communication.\n
    *
    *         'chNum' can take the following values.\n
    *         MCSPI_CHANNEL_n - Channel n is used for communication.\n
    *
    * \return This API will return the status of the McSPI channel status 
    *         register.
    *         User can use the following macros to check the status \n
    *         MCSPI_CH_STAT_RXS_FULL - Receiver register is full \n
    *         MCSPI_CH_STAT_TXS_EMPTY - Transmitter register is full \n
    *         MCSPI_CH_STAT_EOT - End of transfer status \n
    *         MCSPI_CH_TXFFE - FIFO transmit buffer empty status \n
    *         MCSPI_CH_TXFFF - FIFO transmit buffer full status \n
    *         MCSPI_CH_RXFFE - FIFO receive buffer empty status \n
    *         MCSPI_CH_RXFFF - FIFO receive buffer full status \n 
    **/
    unsigned int McSPIChannelStatusGet(unsigned int baseAdd, unsigned int chNum)
    {
        /* Return the status from MCSPI_CHSTAT register. */
        return(HWREG(baseAdd + MCSPI_CHSTAT(chNum)));
    }
    
    /**
    * \brief  This API will enable/disable multiple word OCP access for McSPI 
    *         peripheral.
    *
    * \param  baseAdd        Memory Address of the McSPI instance used.
    * \param  moa            Used to enable/disable MOA in McSPI peripheral.\n
    *
    *         'moa' can take the following values.\n
    *         MCSPI_MOA_ENABLE  - Enable MOA.\n
    *         MCSPI_MOA_DISABLE - Disable MOA.\n
    *
    * \return none. 
    **/
    void McSPIMultipleWordAccessConfig(unsigned int baseAdd, unsigned int moa)
    {
        /* Clear the MOA field of MCSPI_MODULCTRL register. */
        HWREG(baseAdd + MCSPI_MODULCTRL) &= ~MCSPI_MODULCTRL_MOA;
    
        /* Set the MOA fields with the user sent value. */    
        HWREG(baseAdd + MCSPI_MODULCTRL) |= (moa & MCSPI_MODULCTRL_MOA);
    }
    
    /**
    * \brief  This API will enable/disable the FIFO DMA address 256-bit aligned 
    *         feature of McSPI peripheral.
    *
    * \param  baseAdd       Memory Address of the McSPI instance used.
    * \param  fdaa          Used to enable/disable FDAA in McSPI peripheral.\n
    *
    *        'fdaa' can take the following values.\n
    *        MCSPI_FDAA_ENABLE  - Enable FDAA.\n
    *        MCSPI_FDAA_DISABLE - Disable FDAA.\n
    *
    * \return none. 
    **/
    void McSPIFIFODatManagementConfig(unsigned int baseAdd, unsigned int fdaa)
    {
        /* Clear the FDAA field of MCSPI_MODULCTRL register. */
        HWREG(baseAdd + MCSPI_MODULCTRL) &= ~MCSPI_MODULCTRL_FDAA;
    
        /* Set the FDAA field with the user sent value. */
        HWREG(baseAdd + MCSPI_MODULCTRL) |= (fdaa & MCSPI_MODULCTRL_FDAA);
    }
    
    void McSPIPinMuxSetup()
    {
        /*HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_SCLK) = ((0<<0)|(0<<1)|(0<<2)|(1<<5)|(0<<3)|(1<<4));
    
    
        HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_D0) = ((0<<0)|(0<<1)|(0<<2)|(1<<5)|(0<<3)|(1<<4));
    
        HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_D1) = ((0<<0)|(0<<1)|(0<<2)|(1<<5)|(0<<3)|(1<<4));
    
        HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_CS0) = ((0<<0)|(0<<1)|(0<<2)|(1<<5)|(0<<3)|(1<<4));*/
    
        HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_SCLK) =
                             (CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_PUTYPESEL |
                              CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_RXACTIVE);
        HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_D0) =
             (CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_PUTYPESEL |
              CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_RXACTIVE);
        HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_D1) =
             (CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_PUTYPESEL |
              CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_RXACTIVE);
        HWREG(SOC_CONTROL_REGS + CONTROL_CONF_SPI0_CS0) =
                             (CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_PUTYPESEL |
                              CONTROL_CONF_SPI0_SCLK_CONF_SPI0_SCLK_RXACTIVE);
    
    }
    /***************************** END OF FILE ************************************/
    
    
    void SPI0ModuleClkConfig()
    {
        /*HWREG(SOC_CM_PER_REGS + CM_PER_SPI0_CLKCTRL) |=
                CM_PER_SPINLOCK_CLKCTRL_MODULEMODE_ENABLE;
    
             //Waiting for MODULEMODE field to reflect the written value.
           while(CM_PER_SPINLOCK_CLKCTRL_MODULEMODE_ENABLE !=
                  (HWREG(SOC_CM_PER_REGS + CM_PER_SPI0_CLKCTRL) &
                          CM_PER_SPINLOCK_CLKCTRL_MODULEMODE));
    
                   while(CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_SPI_GCLK !=
                  (HWREG(SOC_CM_PER_REGS + CM_PER_L4LS_CLKSTCTRL) &
                  CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_SPI_GCLK));*/
    
    //    HWREG(SOC_CM_PER_REGS + CM_PER_L3S_CLKSTCTRL) =
    //                                 CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
    //
    //        while((HWREG(SOC_CM_PER_REGS + CM_PER_L3S_CLKSTCTRL) &
    //         CM_PER_L3S_CLKSTCTRL_CLKTRCTRL) != CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
    //
    //        HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKSTCTRL) =
    //                                 CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
    //
    //        while((HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKSTCTRL) &
    //         CM_PER_L3_CLKSTCTRL_CLKTRCTRL) != CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
    
            HWREG(SOC_CM_PER_REGS + CM_PER_L3_INSTR_CLKCTRL) =
                                     CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE;
    
            while((HWREG(SOC_CM_PER_REGS + CM_PER_L3_INSTR_CLKCTRL) &
                                       CM_PER_L3_INSTR_CLKCTRL_MODULEMODE) !=
                                           CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE);
    
            HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKCTRL) =
                                     CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE;
    
            while((HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKCTRL) &
                CM_PER_L3_CLKCTRL_MODULEMODE) != CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE);
    
            /*HWREG(SOC_CM_PER_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) =
                                     CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
    
            while((HWREG(SOC_CM_PER_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) &
                                      CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL) !=
                                        CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
    
            HWREG(SOC_CM_PER_REGS + CM_PER_L4LS_CLKSTCTRL) =
                                     CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
    
            while((HWREG(SOC_CM_PER_REGS + CM_PER_L4LS_CLKSTCTRL) &
                                     CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL) !=
                                       CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL_SW_WKUP);*/
    
            HWREG(SOC_CM_PER_REGS + CM_PER_L4LS_CLKCTRL) =
                                     CM_PER_L4LS_CLKCTRL_MODULEMODE_ENABLE;
    
            while((HWREG(SOC_CM_PER_REGS + CM_PER_L4LS_CLKCTRL) &
              CM_PER_L4LS_CLKCTRL_MODULEMODE) != CM_PER_L4LS_CLKCTRL_MODULEMODE_ENABLE);
    
            HWREG(SOC_CM_PER_REGS + CM_PER_SPI0_CLKCTRL) &= ~CM_PER_SPI0_CLKCTRL_MODULEMODE;
    
            HWREG(SOC_CM_PER_REGS + CM_PER_SPI0_CLKCTRL) |=
                                     CM_PER_SPI0_CLKCTRL_MODULEMODE_ENABLE;
    
            while((HWREG(SOC_CM_PER_REGS + CM_PER_SPI0_CLKCTRL) &
              CM_PER_SPI0_CLKCTRL_MODULEMODE) != CM_PER_SPI0_CLKCTRL_MODULEMODE_ENABLE);
    
    
           /* while(!(HWREG(SOC_CM_PER_REGS + CM_PER_L3S_CLKSTCTRL) &
                    CM_PER_L3S_CLKSTCTRL_CLKACTIVITY_L3S_GCLK));
    
            while(!(HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKSTCTRL) &
                    CM_PER_L3_CLKSTCTRL_CLKACTIVITY_L3_GCLK));
    
            while(!(HWREG(SOC_CM_PER_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) &
                   (CM_PER_OCPWP_L3_CLKSTCTRL_CLKACTIVITY_OCPWP_L3_GCLK |
                    CM_PER_OCPWP_L3_CLKSTCTRL_CLKACTIVITY_OCPWP_L4_GCLK)));
    
            while(!(HWREG(SOC_CM_PER_REGS + CM_PER_L4LS_CLKSTCTRL) &
                   (CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_L4LS_GCLK |
                    CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_SPI_GCLK)));*/
    
    }
    
    
    mcspi.h

  • Hi,

    Please reply to above message. I am eagerly waiting.

    Thanks

    Regards

    Gaurav

  • Hi Gaurav,

    Did you get the SPI loopback example working?

    For your code, do you see any activity any of the three SPI pins (SPI_SCLK, SPI_D0, SPI_D1) when you initiate a transfer? 

    I'm reviewing your code, I'll provide feedback soon.

    Regards,
    Frank

  • Gaurav,

    I quickly reviewed your program flow. Overall it looks ok. I have a few questions and observations.

    1. SPI0ModuleClkConfig() & McSPIPinMuxSetup() are APIs you've created? This is probably ok (especially for prototyping & debug), but we encourage use of the board library for module clock and pinmux configuration. Please see http://software-dl.ti.com/processor-sdk-rtos/esd/docs/06_00_00_07/rtos/index_board.html#board-support. Have you checked the proper pinmux settings are applied by your function by inspecting the pinmux registers in the memory map after the function executes?

    2. The remaining API functions are from CSL, so it appears you don't plan to use the SPI LLD? This is OK for a bare metal application.

    3. I notice a few small discrepancies between your program flow and the flow mentioned in the file header for pdk_am335x_1_0_15\packages\ti\csl\src\ip\mcspi\V0\mcspi.h. For example you enable the channel between CS assert & de-assert. I don't think these small differences should cause you to not observe any SPI activity.

    4. You aren't polling Tx / Rx status in your loop before calling McSPITransmitData() & McSPIReceiveData(). I would add this using McSPIChannelStatusGet().

    Regards,
    Frank

  • Frank,

    There is no activity on these three pins (SPI_SCLK, SPI_D0, SPI_D1) in CRO. 

    Yes you are right, I am using for bare metal.

    I am using AM335X_StarterWare_02_00_01_01 as my client wants this.

    I have created SPI0ModuleClkConfig() & McSPIPinMuxSetup(). Can you check this program there on SKAM335x board? If there are any discrepancies in program flow, can you modify the code and send it to me?

    I am doing polling before calling McSPITransmitData() & McSPIReceiveData() as given below, still I am not getting any activity in CRO.

    while(1)

    {
    while(!(HWREG(SOC_SPI_0_REGS + MCSPI_CHSTAT(0))&(1<<1)));
    McSPITransmitData(SPI_BASE_ADD,8,MCSPI_CHANNEL_0);

    ConsoleUtilsPrintf("a1=%d\n",a);

    while(!(HWREG(SOC_SPI_0_REGS + MCSPI_CHSTAT(0))&(1<<0)));
    a=McSPIReceiveData(SPI_BASE_ADD,MCSPI_CHANNEL_0);

    ConsoleUtilsPrintf("a=%d",a);
    }

    Regards

    Gaurav

  • Frank,

    Thanks a lot for helping me. Now SPI is working.

    Regards

    Gaurav