This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSIDK437X: EtherCAT Slave DC issue

Part Number: TMDSIDK437X
Other Parts Discussed in Thread: AM3359

Hello,

I successfully created and compiled the "ethercat_slave_full_AM437x_arm" demo according to the PRU-ICSS Slave User Guide. It works fine when configured with the "Distributed-Clock" set to FreeRun/SM-Synchron. However, as soon as a select the "Distribute-Clock" mode to "DC-Synchron" it can not switch from PreOp->SaveOp->Op. The other commercial device on the bus is able to do this switching (the AM473x is the second device on  the bus). This effect can be discovered with TwinCAT, as well as with the Acontis EC-Engineer and the Acontis EtherCAT Master running on a TMDXIDK5728.

I even tried the MLO and app files from the e2e support thread (e2e.ti.com/.../704543

Can you give me a hint?

Have a nice day,

Bernd