Part Number: AM5749
Other Parts Discussed in Thread: AM5716,
Hello,
I have been trying to set up a boundary scan test on one of our new board configurations that is using the AM5749 processor. I am running into the same signal failures as I see on this AM5716 issue:
https://e2e.ti.com/support/processors/f/791/t/714939
Which correspond to AM5716 errata i928. However, there is no equivalent errata for AM5749.
There is also an additional issue with ddr2_dqs0-3 and ddr2_dqsn0-3. In boundary scan test these are behaving as if they are shorted together even though they are physically separate and not connected to any devices.
I think these issues may be missing errata items, could you please check if you can confirm the behavior?
Thanks,
Josh