Hi,all
I am using TDA2px, it is BIOS.
now all the cores are brought up successfully.
if I set PROC_EVE1_INCLUDE=no,and use DSP A15,it's work ok
but if I set PROC_EVE1_INCLUDE=yes ,(only use EVE1 now), then the board print log is as blow
[HOST] [IPU1-0] 20.667815 s: SYSTEM2: Attaching to [EVE1] ...
[HOST] [IPU1-0] 21.667846 s: SYSTEM2: Attaching to [EVE1] ...
[HOST] [IPU1-0] 22.667876 s: SYSTEM2: Attaching to [EVE1] ...
...
[HOST] [DSP1 ] 25.866955 s: SYSTEM2: Attaching to [EVE1] ...
[HOST] [DSP1 ] 26.866985 s: SYSTEM2: Attaching to [EVE1] ...
[HOST] [DSP1 ] 27.867016 s: SYSTEM2: Attaching to [EVE1] ...
...
[HOST] [DSP2 ] 45.708503 s: SYSTEM2: Attaching to [EVE1] ...
[HOST] [DSP2 ] 46.708534 s: SYSTEM2: Attaching to [EVE1] ...
[HOST] [DSP2 ] 47.708564 s: SYSTEM2: Attaching to [EVE1] ...
Even I didn't run any alg_link at EVE1,but why other core can't attach to EVE1?
Looking forward to your reply
Nigel