Hi:
we are using dpi1 output to ub933 connected ub964 to generate csi2 frame data
Question:
how to configure the vsync&hsync to meet the ub964 timing that hsync should at least tail vsync 5 pclk
here is what we see out lcd1 vsync&hsync
here is camera's vsync&hsync
pVInfo->mInfo.pixelClock = 74500U; pVInfo->mInfo.fps = 60U; pVInfo->mInfo.hBackPorch = 20U;//20U80 pVInfo->mInfo.hSyncLen = 62U; pVInfo->mInfo.hFrontPorch = 20U;//20U48 pVInfo->mInfo.vBackPorch = 12U; pVInfo->mInfo.vSyncLen = 35U; pVInfo->mInfo.vFrontPorch = 6U; pVInfo->vencDivisorInfo.divisorLCD = 1; pVInfo->vencDivisorInfo.divisorPCD = 1;
change above parameter can not delay the vsync&hsync.
any help? Thanks......