Other Parts Discussed in Thread: PMP
I encountered the following error when transplanting uboot. What's the reason?However, these errors do not affect the normal boot of the kernel.Here is the complete print information.
U-Boot SPL 2016.05 (Oct 24 2019 - 11:25:59)
DRA722-GP ES2.0
Trying to boot from MMC1
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
no pinctrl for hs200_1_8v
reading am571x-idk.dtb
reading uImage
spl_load_image_fat: error reading image uImage, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05 (Oct 24 2019 - 11:25:59 +0800)
CPU : DRA722-GP ES2.0
Model: TI AM5718 IDK
Board: AM571x IDK REV
DRAM: 1 GiB
MMC: mmc@4809c000: fail to find sdr104 mode FDT_ERR_NOTFOUND
no pinctrl for sdr104
mmc@4809c000: fail to find ddr50 mode FDT_ERR_NOTFOUND
no pinctrl for ddr50
mmc@4809c000: fail to find sdr50 mode FDT_ERR_NOTFOUND
no pinctrl for sdr50
mmc@4809c000: fail to find sdr25 mode FDT_ERR_NOTFOUND
no pinctrl for sdr25
mmc@4809c000: fail to find sdr12 mode FDT_ERR_NOTFOUND
no pinctrl for sdr12
OMAP SD/MMC: 0, OMAP SD/MMC: 1
1111
444
Warning: fastboot.board_rev: unknown board revision
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:195/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: Could not get PHY for ethernet@48484000: addr 0
eth0: ethernet@48484000
Hit any key to stop autoboot: 2