This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

(D3) TI TDA3x RVP use FPD-Link III output instead of HDMI

Other Parts Discussed in Thread: DS90UB925Q-Q1

Hello,

My predecessor has used the (D3) TI TDA3x RVP with HDMI output. however, for another application, we need the FPD link 3 output of the system. How can I change this?
Also, I'm currently very surprised that the DS90UB925Q-Q1 Serializer delivers a pixel clock of about 150MHz although 85MHz are maximum. Can I configure the Pixel Clock?

>>in the product line data sheet it can be seen that a FPD-Link 3 output is available

Regards,

Burhan