Other Parts Discussed in Thread: OMAP-L138
Hello!
I have to compile php for my board.
Have anybody any success in this?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138
Hello!
I have to compile php for my board.
Have anybody any success in this?
Thanks.
Apache2, yes, as well as other web servers, including Helma which runs under Java. I'll dig a bit into the state of porting PHP.
This thread is a bit old but I'm interested in porting Apache to the dm365. Is there an info on this?
I've just started to port Apache to the DM365. I've noticed that the Montevista binaries for gcc, etc... are misnamed to using the configure application to create the Makefile. Has anyone else tried this port? Or is anyone else doing this now? Perhaps we could share findings.
I did get configure to complete with some assumptions on settings that can't be determined in a cross compile. Now I'm building and see that the XML library libexpat is not built so I need to work on that.
Hi All,
How can I install Nginx and PHP >= 5.5.9 on OMAP-L138 LCDK Linux SDK?
I've setup NFS on ubuntu 16 LTS, so I need install this in /opt/ti/mcsdk_1_01_00_02/targetNFS/ instead of root /var
Thanks
Manish