This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6A816x EVM: Nothing comes out from the UART (p10) port after power on.

Hi,

I have a C6A816x/AM389X EVM, I connected a serial cable between the P10 UART port and my pc, then powered on the evm, but there was nothing come out from the UART port.

If I connect the serial cable to P7, Power Monitor UART, I can see some data printed out, like:

!Power Monitor       0001016mV         0266000uA
#U14 (0V9)           0000912mV         0009000uA
#U11 (1V8 A)         0001804mV         0014000uA
#U7  (1V8 B)         0001812mV         0011000uA
#U59 (VTT/1V5 ALT)   0001500mV         0010800uA
#U22 (3V3)           0003352mV         0216000uA
#U17 (5V0)           0004984mV         0620000uA
#U42 (1V5)           0001804mV         0154400uA
#U23 (1V0 AVS)       0001036mV         0961200uA
#U18 (1V0 CON)       0001016mV         0253600uA
#Expansion 1         0000000mV         0000000uA

I followed the C6A816x_AM389x_EVM_Quick_start_guide to set some switchs on the EMV:

    SW3 (bootmode): BTM0=ON, BTM1=ON, BTM2=ON, BTM3=OFF, BTM4=ON.

    SW4: NAND=OFF, SPI=OFF

Is anybody know what's going on? and also for SW3, how can I change it to boot from tftp/nfs mode?

Thanks!

Mike