Part Number: AM3358
Dear Sir
XGCONF seem to be outdate. I only saw XGCONF for CCV4. It look like I/O with various drivers instead of DEV and GIO in Available Products view. Am I right? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3358
Dear Sir
XGCONF seem to be outdate. I only saw XGCONF for CCV4. It look like I/O with various drivers instead of DEV and GIO in Available Products view. Am I right? Thanks
If my understanding is right, there is the place to choose various drivers in Available Products view. Right now I must use XDCscript Editor to add the drivers. Your documention say GIO will drop. How about DEV? Can I add the driver through DEV? If yes, How to do? Please give the steps as details as possible. If not, what is standard way to add the driver through XGCONF. Thanks
Hi Anping,
Different driver versions can be installed in CCS as follows:
Driver version are selected for a particular project as follows:
XGCONF can be used in CCS 9.0.1 as follows:
I don't think XGCONF can be used for adding required line to .cfg for drivers, and XDCscript Editor (or a text editor) must be used. However, PRSDK contains examples for all drivers which contain the required code. There are also online tutorials which describe how this is done, please see: http://software-dl.ti.com/processor-sdk-rtos/esd/docs/06_00_00_07/rtos/index_faq.html?highlight=training#training-and-documentation
Regards,
Frank
Hi Frank
You wrote
Different driver versions can be installed in CCS as follows:
I saw EDMA3 Low Level Driver, NDK, SYS/BIOS, System Analyzer(UIA Target), XDCtools and am335xPDK. I didn't see the driver UART, McSPI, McASP, I2C and GPIO. Can you tell me how to use DEV? Thanks
Anping,
UART, McSPI, McASP, I2C and GPIO are selected by the PDK (Platform Development Kit) version.
PRSDK drivers aren't DEV/IOM drivers. You should add PRSDK drivers to your application using the approach outlined in the materials I've shared above. I've looped in a colleague to correct me in case I'm wrong about this.
Regards,
Frank
Hi Frank
Because UART, McSPI, McASP, I2C and GPIO are selected by the PDK (Platform Development Kit) version, I can add these drivers by XGCONF! I have verify it. Thanks