Part Number: OMAP-L138
Hi,
After setting PLL0,PLL1, I'm trying additional settings of OCSEL in supervisor mode. But It is set as OSCIN(0x14).
I can't change this register to any other selection like 0x17, 0x18.
Now, OSCDIV is enabled as 0x8000, but OCSEL is not changeable even though on the register view of CCS.
pinmux13 is set to OBSCLK, and I can obserb 24MHz at T18 pin.
Could you give me a piece of advice?
Best Regards,
Tanaka