This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can J7 use the network to communicate between two VM?

Hi, TI team

machine: Ubuntu 18.04

hardware: TI J721E

We want to use the internal tcp/ip network to communicate between two VM.

For application, just create socket for network programming.

Can J7 use the network to communicate between two VM?

Thanks.

Best regards,

Yanhong Chen

  • Hi

    This feature is currently not supported - but we are looking at ways to implement this including options for modeling a virtual network connections built on top of shared memory based IPC mechanism between VM instances

    Dont have a timeline defined for this feature yet