Part Number: AM6548
Other Parts Discussed in Thread: UNIFLASH
Hi
I'm referring http://software-dl.ti.com/processor-sdk-rtos/esd/docs/06_00_00_07/rtos/index_board.html#programming-flashwriter-on-am65xx-platform.
- Close the serial console, disconnect and reconnect the serial cable to USB2UART port (J42) of the board.
I'd like to know the reason why above re-connection of J42 is required.
The error message if I execute "dslite" with the serial console open and without re-connection of J42 is,
Couldn't Open Serial Port!
The error message if I execute "dslite" with the serial console close and without re-connection of J42 is,
Failure:Unknown response from target! Please check the connection!
Failure:Unknown response from target! Please check the connection!” mean?
Q2: Why re-connection of J42 is required?
Q3: Could you modify dslite to be able to run dslite without reconnecting J42?
(This re-connection could be impact at product line.
If I don't do confirmation of character "C" on console then re-connection of J42 is not required.
However, I'd like to request to modify of dslite if it's possible.)
Thanks and Best regards,
HaTa.