Other Parts Discussed in Thread: TMS320F2812
Hi all
I have a very serious problem. Sometime the controller is dead but I don't know the reason.(maybe 1day (24hours) 1 time)
I design my project with the DSP/BIOS and I use Hareware interrupt(250us), Software interrupt(5ms),and SCI, SPI, McBsp,CAN.
The CAN and the SCI are used the Interrupt.
The Semaphore and Que are used various peripheral device.(CANRX, CANTX, SCIRX,SCITX)
- BIOS version is 5.31.02
- Code Generation v4.1.3
Please, help me