Part Number: AM5728
hello
when I connect my EVM (TMDSEVM572x) to PC by LAN cable and run command ifconfig, what is seen is only IPv6, not IPv4.
I use serial cable and minicom terminal to connect to EVM.
I executed command ifconfig on EVM via minicom as follows:
root@am57xx-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr FC:0F:4B:AB:9B:38
inet6 addr: fe80::fe0f:4bff:feab:9b38/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:220 errors:0 dropped:0 overruns:0 frame:0
TX packets:126 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:41109 (40.1 KiB) TX bytes:28382 (27.7 KiB)
Interrupt:90
eth1 Link encap:Ethernet HWaddr FC:0F:4B:AB:9B:39
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:107 errors:0 dropped:0 overruns:0 frame:0
TX packets:107 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:202696 (197.9 KiB) TX bytes:202696 (197.9 KiB)
as you can see above, only inet6 detected and has IP.
I need to know EVM's IPv4 for connecting via CCS RSE and debuging codes.
any help would be appreciated,
Ali