Hi,
Has PRU-ICSS Ethernet Switch firmware been tested on AM57xx ? Is there any example project of PRU-ICSS Ethernet Switch including each source code ? We’re looking into 7.1 Dual EMAC and Switch in Processor SDK RTOS Software Developer’s Guide below.
http://software-dl.ti.com/processor-sdk-rtos/esd/docs/06_01_00_08/rtos/index_pru_icss_fw.html#switch
However, only document of ICSS SWITCH FIRMWARE Design Guide is described in 7.1.7. Running ICSS-EMAC FIRMWARES Example.
Also, the section of EMAC and Switch in Processor SDK RTOS ICSS-EMAC-Design describes as follows;
The icss_emac LLD only provides a simple EMAC loopback example, right now there is no example for a standalone switch on the lines of EMAC.
http://processors.wiki.ti.com/index.php/Processor_SDK_RTOS_ICSS-EMAC-Design#EMAC_and_Switch
Could you tell us where we can get an example project ?
We prefer AM57xx IDK, but AM335x would be OK.
By the way, the following Industrial SW are using the above PRU-ICSS Ethernet Switch firmware ?
PRU-ICSS-ETHERCAT-SLAVE
PRU-ICSS-ETHERNETIP-ADAPTER
PRU-ICSS-PROFINET-SLAVE
Thanks and regards,
Hideaki