This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Re: C6A8 EVM BSP/CSL



However, there are still csl files that are needed specifically for the C6A8 that are not in OMAP.  Plus, the hardware addresses are different for the peripherals for the two different chips.  So a different csl is needed to define those addresses.  For example, I cannot find the csl for the EMAC Control Module (e.g., register CMMISCINTEN).  I'm sure others are missing too.  I installed the ezsdk_c6a816x-evm_5_00_00_56_setuplinux package, but it doesn't appear to have the C6A8 specific csl.

So my question for some TI Employee is, is all the supporting software for Integra available now.  Has it been published.  If so, where is it.  Right now is Integra (peripheral) support where OMAP support was 4-5 years ago.

Thank you.