Hello,
We use tda2hg device based on VSDK 03 05.We set it as Linux + BIOS mode. It can not support 'ps -ef' command in shell, but 'ps -l' is normal. We need 'ps -ef' command, how do we do? Could you help to have a look?
=====================================================
root@dra7xx-evm:~# ps -ef
ps: invalid option -- 'e'
BusyBox v1.24.1 (2018-09-17 14:56:41 IST) multi-call binary.
Usage: ps
root@dra7xx-evm:~# ps -l
S UID PID PPID VSZ RSS TTY STIME TIME CMD
S 0 1 0 5076 4188 0:0 09:22 00:00:04 {systemd} /sbin/init
S 0 2 0 0 0 0:0 09:22 00:00:00 [kthreadd]
S 0 3 2 0 0 0:0 09:22 00:00:00 [ksoftirqd/0]
S 0 4 2 0 0 0:0 09:22 00:00:02 [kworker/0:0]
S 0 5 2 0 0 0:0 09:22 00:00:00 [kworker/0:0H]
S 0 6 2 0 0 0:0 09:22 00:00:00 [kworker/u4:0]
S 0 7 2 0 0 0:0 09:22 00:00:00 [rcu_preempt]