Part Number: PROCESSOR-SDK-DRA7X
Other Parts Discussed in Thread: DRA742, PMP
Hi,
I have trying to boot the board from SD card but it is showing
U-Boot SPL 2016.05-g333293e877 (Dec 28 2017 - 05:17:21)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
** First descriptor is NOT a primary desc on 0:1 **
*** Warning - MMC init failed, using default environment
Trying to boot from MMC1
*** Warning - MMC init failed, using default environment
** Partition 1 not valid on device 0 **
spl_register_fat_device: fat register err - -1
spl_load_image_fat: error reading image u-boot.img, err - -1
*** Warning - MMC init failed, using default environment
spl: no partition table found
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
If I do CPU Reset below log it is showing
Hit any key to stop autoboot: 0
** First descriptor is NOT a primary desc on 0:1 **
switch to partitions #0, OK
mmc0 is current device
** First descriptor is NOT a primary desc on 0:1 **
SD/MMC found on device 0
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** First descriptor is NOT a primary desc on 0:1 **
switch to partitions #0, OK
mmc0 is current device
** First descriptor is NOT a primary desc on 0:1 **
SD/MMC found on device 0
** No partition table - mmc 0 **
switch to partitions #0, OK
mmc1(part 0) is current device
mmc - MMC sub system
How to solve this.
Thank you,
Deepthi