This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuration Aptina CMOS Sensor MT9P031

Hello everyone

I be developing my application with the microprocessor 365, and are using the Aptina sensor, CMOS MT9P031.

I want to change some configuration parameters of the sensor. Right now, the sensor is configured as image capture, "binning"and I want to use the mode "window. " I also want to change the orientation of the sensor, from horizontal to vertical.

How I can modify? Where are the files that have sensor configuration?

I be using 2.1 dvsdk

Thank you very much everybody.