This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM5728: pdkProjectCreate not working without edma3

Part Number: AM5728
Other Parts Discussed in Thread: CCSTUDIO

Tool/software: Code Composer Studio

Using version 

When trying to run pdkProjectCreateI get the following error:

andre@andre-ubuntu-VirtualBox:~/ti/pdk_am57xx_1_0_16/packages$ ./pdkProjectCreate.sh AM572x evmAM572x little spi all dsp
=========================================================================
Configuration:
SOC : AM572x
BOARD : evmAM572x
ENDIAN : little
MODULE : spi
PROJECT_TYPE : all
PROCESSOR : dsp
PDK_SHORT_NAME : /home/andre/ti/pdk_am57xx_1_0_16/packages
=========================================================================
Checking Configuration...
PDK_PARTNO : AM572X
PDK_ECLIPSE_ID : com.ti.pdk.am57xx
RTSC_PLATFORM_NAME : ti.platforms.evmAM572X
RTSC_TARGET : ti.targets.elf.C66
CCS_DEVICE : com.ti.ccstudio.deviceModel.C6000.GenericC64xPlusDevice
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace /home/andre/ti/pdk_am57xx_1_0_16/packages/MyExampleProjects
Detected Project ./MCSPI_Loopback_evmAM572x_c66xExampleProject.txt

--------------------------------------------------------------------------------
Creating project 'MCSPI_Loopback_evmAM572x_c66xExampleProject'...

NOTE: Compiler version '8.3.2' is not currently installed! - defaulting to '8.3.3'.

!ERROR: Unknown product-type ID 'com.ti.sdo.edma3'!
NOTE: Refer to the following list of available product-type IDs (the display-names in square brackets are for reference only):

com.ti.rtsc.openmp [am57xx OpenMP]
com.ti.pdk.am57xx [am57xx PDK]
com.ti.ctoolslib [CTools Library]
ti.mas.dsplib.c66x [DSPLIB C66x]
com.ti.rtsc.FrameworkComponents [Framework Components]
ti.imglib.c66x [IMGLIB C66x]
com.ti.rtsc.IPC [Inter-processor Communication]
ti.mas.mathlib.c66x [MATHLIB C66x]
com.ti.rtsc.NDK [NDK]
com.ti.rtsc.SYSBIOS [SYS/BIOS]
com.ti.uia [System Analyzer (UIA Target)]
com.ti.rtsc.XDAIS [XDAIS]
com.ti.rtsc.XDCtools [XDCtools]

Job found still running after platform shutdown. Jobs should be canceled by the plugin that scheduled them during shutdown: com.ti.ccstudio.devicemodel.DeviceModelLoader$InitializationJob$3
Copying macros.ini
Project generation complete
*****************************************************************************

It turns out that the edma3 library was not automatically added to CCS for some reason. I had to manually add the EDMA library to correct this error.