Other Parts Discussed in Thread: AM3517
As far as I can tell none of the new (or old) demo NK.bin's for AM3517 EVM support code development with C#.
Looks like the cab file with .NETCF 3.5 update doesn't work when Visual Studio tries to load it and it is not part of the build. I have Active Sync working and device setup done. Just looks like only C++ development is supported.
1) is this correct or am I making some mistake ?
2) are there any notes (like in user guide) on what catalog items, etc. are needed to make sure C# code can run on the EVM ?
I'm asking as I have errors when building the AM35x_OSDesign so can't generate my own NK.bin right now and wanted to allow other developers to use some of the AM3517 EVM kits before I figure out the problem with building NK.bin.