I have got the TPS659101 samples,but what I need is TPS65910.
CPU is AM3517.
SO question is:
When set BOOT[0:1]=00,will the TPS659101 become same as TPS65910?
if so ,I can use TPS659101 to power the AM3517.
please help me ASAP,thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Yes, you are right. These two devices are identical except for the power-up sequence.
With AM3517 you can use the boot sequence as you have mentioned.
Regards,
Gandhar.