“- Fixed syntax errors in tsp659xx MUSB OTG transceiver support. Note that this feature is untested and unsupported.”
I found this line in the "readme.txt" under the folder "TI_EVM_3530". So what's the status now? Because we're just using this HW configuration(HSUSB0 port on OMAP3530, TPS65930 as PHY) in our design, I'm afraid there're some issues we can't handle and there is no support at all.