ecspi1: ecspi@02008000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6ul-ecspi", "fsl,imx51-ecspi";
reg = <0x02008000 0x4000>;
interrupts = <GIC_SPI 31 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_ECSPI1>,
<&clks IMX6UL_CLK_ECSPI1>;
clock-names = "ipg", "per";
dmas = <&sdma 3 7 1>, <&sdma 4 7 2>;
dma-names = "rx", "tx";
status = "disabled";
};
pinctrl_ecspi1: ecspi1grp {
fsl,pins = <
MX6UL_PAD_LCD_DATA22__ECSPI1_MOSI 0x100b1
MX6UL_PAD_LCD_DATA20__ECSPI1_SCLK 0x100b1
MX6UL_PAD_LCD_DATA23__ECSPI1_MISO 0x100b1
MX6UL_PAD_UART1_RTS_B__GPIO1_IO19 0x80000000 /* PN5180 nRST */
>;
};
&ecspi1 {
fsl,spi-num-chipselects = <1>;
/* cs-gpios = <&gpio3 26 0>; */
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
status = "okay";
};
i am getting error as
Error: arch/arm/boot/dts/imx6ull-iwg26.dts:91.17-26 syntax error
FATAL ERROR: Unable to parse input tree
make[1]: *** [arch/arm/boot/dts/imx6ull-iwg26.dtb] Error 1
make: *** [dtbs] Error 2
how to resolve it